2013-07-22 9:28 AM
Hi all!
I'm new in forum. I wrote this config for I2S. Instead of MCLK=256*Fs=12, 288000 MHz and CK=48KHz*32bit*2channel=3, 072000 MHz, I measured MCLK=4MHz and CK=1 MHz. My code is:RCC_APB1PeriphClockCmd (RCC_APB1Periph_SPI2, ENABLE);
// ..................../* Connect pins to I2S peripheral */
GPIO_PinAFConfig (PCM1804_PORTC, PCM1804_SCKI_PS, GPIO_AF_SPI2); // I2S2_SCKI GPIO_PinAFConfig (PCM1804_PORTB, PCM1804_I2S2_CK_PS, GPIO_AF_SPI2); // I2S2_CK GPIO_PinAFConfig (PCM1804_PORTB, PCM1804_I2S2_SD_PS, GPIO_AF_SPI2); // I2S2_SD GPIO_PinAFConfig (PCM1804_PORTB, PCM1804_I2S2_LRCK_PS, GPIO_AF_SPI2); // I2S2_LRCK , WS // I2S2 peripheral configuration I2S_InitTypeDef I2S2_InitStructure; SPI_I2S_DeInit (SPI2); /* For this standard, the WS signal is used to indicate which channel is being transmitted. It is activated one CK clock cycle before the first bit (MSB) is available. */ I2S2_InitStructure.I2S_Standard = I2S_Standard_Phillips; I2S2_InitStructure.I2S_DataFormat = I2S_DataFormat_24b; I2S2_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Enable; I2S2_InitStructure.I2S_AudioFreq = I2S_AudioFreq_48k; // I2S2_InitStructure.I2S_CPOL = I2S_CPOL_Low; // I2S2_InitStructure.I2S_Mode = I2S_Mode_MasterRx; // I2S_Init (SPI2, &I2S2_InitStructure); /* I2S_INTERRUPT */ NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = SPI2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init (&NVIC_InitStructure); /* Enable the Rx buffer not empty interrupt */ SPI_I2S_ITConfig (SPI2, SPI_I2S_IT_RXNE, ENABLE); // I2S clock configuration in system file is:/************************* PLL Parameters *************************************/
/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */
#define PLL_M (uint32_t)8
#define PLL_N (uint32_t)336
/* SYSCLK = PLL_VCO / PLL_P */
#define PLL_P (uint32_t)2
/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */
#define PLL_Q (uint32_t)7
/* PLLI2S_VCO = (HSE_VALUE Or HSI_VALUE / PLL_M) * PLLI2S_N
I2SCLK = PLLI2S_VCO / PLLI2S_R */
#define PLLI2S_N (uint32_t)258
#define PLLI2S_R (uint32_t)3
//.................
/******************************************************************************/
/* I2S clock configuration */
/******************************************************************************/
/* PLLI2S clock used as I2S clock source */
RCC->CFGR &= ~RCC_CFGR_I2SSRC;
/* Configure PLLI2S */
RCC->PLLI2SCFGR = (PLLI2S_N << 6) | (PLLI2S_R << 28);
/* Enable PLLI2S */
RCC->CR |= ((uint32_t)RCC_CR_PLLI2SON);
/* Wait till PLLI2S is ready */
while((RCC->CR & RCC_CR_PLLI2SRDY) == 0)
{
}
On disvovery board the oscillator frequency is 8MHz, and in stm32f4xx.h the HSE value is:
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t)8000000) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */
Thank you !
Regards
uprog
#stm32f4-i2s
2013-07-28 8:17 AM
Hi !
I didnt found any solution yet. I use GCC configured with:../gcc-linaro-4.6-210/configure
--target=arm-none-eabi --prefix=/opt/ARM/arm-linaro-eabi-4.6/ --enable-multilib --enable-languages=c,c++ --with-newlib --with-gnu-as --with-gnu-ld --disable-nls --disable-shared --disable-threads --with-headers=newlib/libc/include --disable-libssp --disable-libstdcxx-pch --disable-libmudflap --disable-libgomp --disable-werror --with-system-zlib --disable-newlib-supplied-syscalls<br>Thread model: single<br>gcc version 4.6.2 20111004 (prerelease) (Linaro GCC 4.6-210)
And:
CFLAGS = -I. -IInclude -Iinclude -Iinc \<br> -c -fno-common -O2 -g -D
''assert_param(x)=''
-DARM_MATH_CM4 \<br> -mcpu=cortex-m4 -mthumb \<br> -mfloat-abi=hard -mfpu=fpv4-sp-d16 \<br> -fsingle-precision-constant #\
2013-07-29 9:27 AM
And what is the content of SPI_I2SPR after the setup?
JW2013-07-29 1:37 PM
Hi !
I don't know, because I have used a precompiled std. periph. static library and I can't watch the SPI_I2SPR register content. Regards uprog2013-07-29 1:40 PM
Or print them via a console, or SWD?
If you can't get you debugger to dump arbitrary memory locations, you might want to find some different tools. The PLL setting looked to be reasonable.2013-07-30 2:59 AM
> I don't know,
And how are we then supposed to know? Although, in fact, we are not interested. *You* are. It was a hint that *you* should investigate the setting of this register. > because I have used a precompiled std. periph. static library Then don't. It might've been compiled with unexpected settings (e.g. with I2S_EXTERNAL_CLOCK_VAL set). > and I can't watch the SPI_I2SPR register content. You always can read it out after it has been set. You can also look at the disassembled binary. JW2013-10-16 4:44 AM
With Keil it's working fine ! I have 256x48 kHz MCK clock signal.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.