STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with i2s configuration

Posted on April 02, 2014 at 12:05hello everyonei have adc ad1877, configured as in pictureHow i should configure i2s in stm32f4 ? I have tried this one   I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_32k;  I2S_InitStructure.I2S_Standard = I2S_Stan...

0690X000006056mQAA.png
silent by Associate II
  • 5125 Views
  • 14 replies
  • 0 kudos

STM32F4 User Push Button Interrupt Issue

Posted on April 06, 2014 at 05:22 Hey, I'm currently working on a project for my class with the STM32F4 board, and am having difficulty trying to configure the user push button to cause an interrupt. I have used the F3 board a few times, ...

DAC/ADC/SPI Comm. - Timing Analysis

Posted on April 03, 2014 at 20:53All, We are using the STM32F051C8T6.I have some comments and questions below but I mainly wanted to get a thumbs up to make sure I was on the right track with some of my conclusions.  Thank you for taking the time t...

0690X00000602mCQAQ.jpg 0690X00000602rzQAA.jpg 0690X00000602s4QAA.jpg 0690X00000602s9QAA.jpg

Curve fitting libraries

Posted on April 04, 2014 at 18:31Hi,I am currently working on a PIR-sensor solution, where 10 PIR-sensors are mounted in an array containing lets say 300 elements, at an even spacing distance.Looks like this:* = PIR♯ = array element without PIR-sens...

matte by Associate II
  • 1924 Views
  • 1 replies
  • 0 kudos

stm32f4discovery can write/read flash but not work

Posted on April 04, 2014 at 17:40After days spent in tries to connect adc via i2s - mcu stopped working. I can write and read flash via st-link, mcu is properly detected but it does nothing. Tried mass erase - did not helped.It seems that works only...

silent by Associate II
  • 3438 Views
  • 9 replies
  • 0 kudos

UART4 DMA Rx Problem

Posted on April 04, 2014 at 13:21I cannot get into DMA mode, the code  I wrote did not get into DMA  interrupt. The code I wrote is as follows. Any advice?( my processor is STM32F103ZG) uint8_t RxBuffer1[100];  /*UART - Pin Config*/  GPIO_InitTypeDe...

Interrupt nesting problem

Posted on April 04, 2014 at 17:26Hi, I am trying to get interrupt nesting to work on an STM32F207, but so far without success. I am using no subpriorities (SCB_AIRCR.PRIGROUP = 3) I am inside the hander of TIM6_DAC, and an UART5 interrupt is enabled...

zabel by Associate III
  • 794 Views
  • 1 replies
  • 0 kudos

STM32F405 MEDIANFILTER

Posted on April 04, 2014 at 13:03Hey, Does anybody know a DSP-Function for a medianfilter? with filterlength of 5 points. At the moment I have written the filter with for-loops, and it is too slow for my application. Thank you, Michael #m

um0794 source code

Posted on March 15, 2011 at 16:40UM0794: GSM interfaceI can not find um0794.zip. Help me please.

vldm by Associate
  • 1167 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.