STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX - Configuration Bug?

Posted on April 07, 2014 at 14:40Hello, I wish to use the STM32F4Discovery board by using STM32CubeMX for MCU as configuration tool and Keil - MDK for code programming/debuging. The problem appear when HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_L...

0690X00000603QLQAY.jpg 0690X00000603IXQAY.jpg 0690X00000603QQQAY.jpg 0690X00000603QVQAY.jpg
dorin by Associate
  • 939 Views
  • 2 replies
  • 0 kudos

Interruption on internal event

Posted on April 07, 2014 at 10:56Hey. I have a big project that I am working on with STM32F4-Discovery board and I need to use interruptions requested by internal events ( not Timers ) such as variables changing. Can anyone help me with that? Thank ...

mejrissi by Associate II
  • 1644 Views
  • 2 replies
  • 0 kudos

TIM10 LSI

Posted on March 24, 2014 at 15:39 I'm working with STM32L151, and I'm trying to set the LSI clock as Timer 10 source. I tryed the following configuration but it didn't work properly (counts at system clock frequency). Can anyone help me to find t...

tg22410 by Associate II
  • 3329 Views
  • 7 replies
  • 0 kudos

USART Help

Posted on April 06, 2014 at 03:23I'm using a STM32F3 Discovery and connecting it to labVIEW the problem is that I can't receive more than one byte. Can someone help me modifying my code to allow multiple byte reception. I'm testing it sending someth...

STM32F4 Discovery HD44780 4bit mode

Posted on June 16, 2012 at 22:38 Can't seem to get any text output using the 4 bit mode of the chip (managed to get 8bit mode). Tried following the HD44780/SPLC780D datasheets to no avail. Here's my code. Hope someone can help as I've been strug...

STM32F103RET6 ADC reads voltage with no voltage at pin

Posted on April 06, 2014 at 20:01 If i read any of the ADC's i see a voltage of about 1736mv it changes a little depending on the sampling speed, i've used non continuous reads, and continuous DMA , both mostly the same, reads the same in circui...

charlie2 by Associate II
  • 888 Views
  • 2 replies
  • 0 kudos

STM32F0 - SPIRIT1

Posted on January 18, 2013 at 17:03Hi, I work with STM32F0, I connect this to SPIRIT1.I need assistance of ST, because I have difficult to work spirit1. I read and write register of SPIRIT1 with successfully. I use the library of ST for work with sp...

STM32F205 fails after setVectorTable call

Posted on April 04, 2014 at 22:43 There is something basic I am overlooking but haven't been able to figure out what. I've written a bootloader that seemed to work, but maybe it just happened to fall into the new program. I seem ...

vneff by Associate III
  • 2152 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.