2014-04-04 9:31 AM
Hi,
I am currently working on a PIR-sensor solution, where 10 PIR-sensors are mounted in an array containing lets say 300 elements, at an even spacing distance.Looks like this:* = PIR♯ = array element without PIR-sensor.*♯♯♯♯*♯♯♯♯*♯♯♯♯*♯♯♯♯*...The PIR-sensors are supposed to detect when a person moves alongs this array. I can only use ~10 sensors and therefore need to guess whether a person is present in between 2 sensors and if so, where he/she actually is standing.So I have 10 data points where I know the X-value (the position in the array of these sensors) and I can read the corresponding Y-values from these PIR-sensors.Now how do I achieve a curve fitting. I am thinking that cubical spline or polynomial interpolation are the best two methods for this specific applicaiton. I need a library that can interpolate the rest of the array elements which are unknown. Any ideas of where I can find this?I intend to use and STM32F4-Discovery board to read the sensors and perhaps the FPU/DSP to calculations. #stm32f4 #curve-fitting2014-04-05 3:53 AM
I think that once you have read the sensors and put their values into an array of floats, you are sufficiently far from the hardware that a generic solutions book e.g. in C is the right approach.
My favourite book for such things is ''Numerical Recipes'' as they don't just give you some code, they try to explain why a given approach is good and when to choose something else. Translations are available for various different programming languages; according to amazon the C version is in its third edition. Hope this helps, DanishWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.