STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EmberZNet Stack 4.3.0

Posted on April 10, 2013 at 13:22Is this EmberZNet Stack 4.3.0 file downloadable from ST website? I need this for setting up a mesh network on STM32W RF Control Kit. If someone of you have this file. please update somewhere on the web. Regards, ns ...

enes by Associate II
  • 4324 Views
  • 9 replies
  • 0 kudos

Polarity PWM on STM32F4

Posted on April 08, 2014 at 16:03 Hello! I am trying to create two square PWMs (duty 50%) with a controlled phase shift (0° to 90°). I am currently using TIM4 with 2 channels set on TIM_OCMode_Toggle and it is working OK. The pro...

thoman92 by Associate
  • 1638 Views
  • 2 replies
  • 0 kudos

I2C SDA, SCL held high

Posted on April 08, 2014 at 15:37 I m working on STM32F303. I have interfaced I2C2 to EEPROM and DS3231 with pullups on SDA and SCL..Issue: After Reset, SDA and SCL line is held high (it only happens ocassionally)..While I2C works properly, i can ac...

STM32 standard peripheral library

Posted on April 07, 2014 at 13:55I'm using the STM32f107, and trying to write simple code to output a DC level from the DAC. I have the User Manual UM0427, revision 5 October 2007.  This revision is missing the DAC section.  I cannot find a later ve...

mike2399 by Associate II
  • 1209 Views
  • 2 replies
  • 0 kudos

STM32Cube MD5 error when loading FW1.1.0

Posted on April 08, 2014 at 10:44Hi all, When i launch ''generate code'', MXCube say me ''The firmware package ... v1.1.0 is not available in your repository ...do you want to download this now ?'' ... Yes A popup appear and say ''Problem diuring do...

tgoin by Associate II
  • 1236 Views
  • 2 replies
  • 0 kudos

STM32cubeF4 doesn't include CMSIS DSP...

Posted on April 04, 2014 at 16:20... (yet?) or am I not looking in the right place? I have FW version 1.1.0. Can anyone confirm that this is the case? Donald

d_1 by Associate II
  • 1329 Views
  • 1 replies
  • 0 kudos

ADC capture triggered by tim STM32 discovery

Posted on April 07, 2014 at 16:42Hey everyone! I am new to working with the STM32F429 discoveryboard and can't seem to find a solution for sampling with the ADC via the DMA at 160Khz (I am trying to sample a 40kHz wave). Does anyone have any ideas o...

thorin by Associate
  • 1089 Views
  • 1 replies
  • 0 kudos

NVIC Priority Groups

Posted on April 07, 2014 at 14:48I have read through Yiu's Cortex M3 book on the NVIC, and read this section of the COrtex M3 manual (http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0337e/ch05s03s02.html), and am still missing the ans...

jvavra by Associate III
  • 1243 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.