2014-04-07 5:48 AM
I have read through Yiu's Cortex M3 book on the NVIC, and read this section of the COrtex M3 manual (
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0337e/ch05s03s02.html
), and am still missing the answer to one vital, basic question: does the Priority Group have any bearing on the actual priority assigned to an IRQ, or do the groups just allow you to have available different numbers of preemptive priorities/subpriorities? So for example, if I want 16 subpriorities, I have to use Group 0, as its the only group with 4 bits available for subpriorities. But if I've assigned an IRQ to Group 0, subpriority 0, is this necessarily higher than one assgined to Group 1, pre-emption priority 0, subpriority 0? If not, how are these arbitrated? EDIT: Or, do I assign a Preemption Priority to a particular group (which could be any of the four), and the IRQs that are then included in that group would all have the same preemption priority (but possibly different subpriorities)?2014-04-07 7:45 AM
Priority is controlled by the sub-priority, and the NVIC# when that is ambigous.
If you want specific interrupts to break into others, they must have a lower pre-emption level. Otherwise the ordering is managed as the interrupt exits, and the processor makes a tail-chaining decision. Ideally your interrupts should be brief and simple, if things will take a long time queue the work so it can be handled in a deferred manner. This can avoid a lot of grief with priorities, and priority inversions when resources are locked.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.