2014-04-07 7:42 AM
Hey everyone! I am new to working with the STM32F429 discoveryboard and can't seem to find a solution for sampling with the ADC via the DMA at 160Khz (I am trying to sample a 40kHz wave). Does anyone have any ideas on what in my approach that is incorrect?
Code used:/*♯♯-1- Configure the ADC peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ AdcHandle.Instance = ADCx; AdcHandle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2; AdcHandle.Init.Resolution = ADC_RESOLUTION12b; AdcHandle.Init.ScanConvMode = DISABLE; AdcHandle.Init.ContinuousConvMode = ENABLE; AdcHandle.Init.DiscontinuousConvMode = DISABLE; AdcHandle.Init.NbrOfDiscConversion = 0; AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; AdcHandle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_CC1; AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT; AdcHandle.Init.NbrOfConversion = 1; AdcHandle.Init.DMAContinuousRequests = ENABLE; AdcHandle.Init.EOCSelection = DISABLE;/*♯♯-2- Configure ADC regular channel ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ sConfig.Channel = ADCx_CHANNEL; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; sConfig.Offset = 0; if(HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK) { /* Channel Configuration Error */ Error_Handler(); }/* Enable HSE Oscillator and activate PLL with HSE as source */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 16; RCC_OscInitStruct.PLL.PLLN = 360; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 0; HAL_RCC_OscConfig(&RCC_OscInitStruct); HAL_PWREx_ActivateOverDrive(); RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4);}//TIMER INITvoid TIM3_Config(void){ static TIM_HandleTypeDef htim; TIM_MasterConfigTypeDef sMasterConfig; /*♯♯-1- Configure the TIM peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ /* Time base configuration */ htim.Instance = TIM3;// htim.Init.Period = 799; // htim.Init.Period = 374; //test f�r 180MHZ klockfrekvens htim.Init.Period = 74; htim.Init.Prescaler = 0; htim.Init.ClockDivision = 0; htim.Init.CounterMode = TIM_COUNTERMODE_UP; HAL_TIM_Base_Init(&htim); /* TIM6 TRGO selection */ sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; HAL_TIMEx_MasterConfigSynchronization(&htim, &sMasterConfig); /*♯♯-2- Enable TIM peripheral counter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ HAL_TIM_Base_Start(&htim);} #adc #tim #stm322014-04-07 8:00 AM
Not much interest for the Cube library from me, the STM32F429I-DISCO has limited ADC channels, I have posted examples for it, but mostly for the F2/F4 platform.
I posted a 200 KHz example about a third down [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Help%20with%20simple%20ADC%20on%20STM32F4&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=3749]This ThreadWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.