STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Input Capture on both edges to detect signal duration

Posted on May 17, 2014 at 00:52 Hi, I am trying to get the duration of a signal with input capture of timer. I have two signals, which are comming from another chip, CLK and OUT. CLK is 125 KHz and OUT is variable between ~3.5KHz and 4KHz....

STM32F401RE Nucleo VCP Problems on Win XP

Posted on April 23, 2014 at 19:00Using Win XP. I've installed the latest firmware in my Nucleo board (LINK007). I've installed the drivers on my PC (LINK009). All is well with the USB Mass Storage but the VCP has a yellow '?' in the device manager w...

0690X00000603HJQAY.jpg
ve7su by Associate II
  • 3374 Views
  • 8 replies
  • 0 kudos

STM32F373CCT6 SPI issues

Posted on May 16, 2014 at 17:55I am having issues with SPI1 and SPI2 on the STM32F373CCT6 chip. 1) I have both busses configured the same as full duplex, 16 bit data, master mode, baud rate scaler of 8.  However, when I look at the SPI clocks on a s...

jprinster by Associate II
  • 1793 Views
  • 3 replies
  • 0 kudos

STM32F3 ADC/DMA problem

Posted on May 15, 2014 at 15:58  The original post was too long to process during our migration. Please click on the attachment to read the original post.

Switch statement error

Posted on May 15, 2014 at 18:09Hi I just can't understand this... So, I'm communicating with PC's terminal program via USART2 on my STM32F10. Communication is running smoothly both ways, but I have a problem when I want my embedded system to respond...

0690X00000605YMQAY.png
codium by Associate II
  • 5032 Views
  • 8 replies
  • 0 kudos

Interrupts and loss of Data

Posted on May 15, 2014 at 19:35I am currently building a big project on STM32F4 Discovery board for my graduation project. I have configured 4 Timers' interrupts (10Hz, 50Hz, 100Hz and 1kHz), USART communication with interrupt, and CAN communication...

mejrissi by Associate II
  • 4606 Views
  • 9 replies
  • 0 kudos

RTC Flags problem when alarm is set

Posted on May 16, 2014 at 13:37 Hi, My RTC (F103) is currently running from LSI. The counter is counting properly, and the SEC flag in CRL is set every second as expected. When the Alarm is set, the SEC flag is asserted and cannot be c...

STM32F05x SPI clk single bit

Posted on May 14, 2014 at 17:07 Hi, I have a PCB with a STM32F051 connected to 3 ADCs ( http://datasheets.maximintegrated.com/en/ds/MAX11166-MAX11pdf) in daisy chain. Page 29 Figure 14 of the datasheetshows the schematic I implement...

aoleon by Associate II
  • 2879 Views
  • 4 replies
  • 0 kudos

usb library on windows 7 (does not work)

Posted on May 01, 2014 at 18:46I am trying to use the usb library found here:  http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257882#I am on windows 7, I am using the port207z board here with the STM32f207z: http://www.wvshare.com/p...

epataky by Associate II
  • 1659 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.