STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 Bootloader Read Memory command failed

Posted on May 19, 2014 at 16:33I am trying to use the ST Flash loader software for download STM32F401 and there is a problem when the software tries to read the address 0x1FFF7A22 (contained flash size) and 0x1FFF7A10 (unique device ID). It seems th...

laetitia by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

STM32F4 Bug with SPI1

Posted on September 23, 2012 at 22:17I am having a strange issue. I am using FatFS and I have setup the SPI1 withCS - PB14CK - PA5MISO - PA6MOSI - PA7When I just use the SD card interface, everything works well. I am getting the proper SPI signals a...

STM32F207 FSMC connected to especially device

Posted on May 14, 2014 at 11:53I have a question about connecting specially device to a FSMC interface on STM32F207IGT6. There is some points describing this case it bellow.-          MCU:                   STM32F207IGT6 -          DEVICE:          ...

kruzicka by Associate II
  • 1268 Views
  • 3 replies
  • 0 kudos

STM32F207 ETH clock

Posted on May 14, 2014 at 11:54Hello, I've problem with a clock setting for a MCU. There is some points, which describe it. General: MCU: STM32F207IGT6 Clock: HSE 8Mhz -> PLL 96Mhz Using module: ETH MAC - MII 4-bit mode - 25MHz neededFSMC - synchro ...

kruzicka by Associate II
  • 1197 Views
  • 2 replies
  • 0 kudos

Trigger interrupts for ETR

Posted on May 18, 2014 at 14:10Hi! (Using the STM32F103RBT6 chip) I've configured TIM2 timer as a prescaler for TIM3 (RM0008 page 386). Timer TIM2 is configured for ETR (RM0008 page 365). So what I've got is a 32bit timer counting pulses on PA0 (suc...

gor by Associate
  • 1994 Views
  • 3 replies
  • 0 kudos

STM32F303xC bootloader

Posted on May 16, 2014 at 16:12Hi everyone, i'm trying to enter bootloader from my application, so i could use STM flash loader tool to upgrade software. Everything is working fine and im entering bootloader, but after i flash with flash loader tool...

STM32F205RBT6 does not start sometimes on power up

Posted on May 18, 2014 at 14:46I am using STM205RBT^ & I have noticed that it does not start executing first instruction sometimes. I am using HSI oscillator & used pll to make 120Mhz. My first line in code is to toggle a pin. Only two possibilities...

stm32f40x discovery TIM9 and TIM12 PWM input capture

Posted on April 23, 2014 at 15:33hi all,   I'm new in the forum and I am experiencing a problem of ISR , which doesn't  happen for TIM12 while, with same ch1 configuration register and same pwm signal input,  set the ISR calling for TIM9, as expecte...

philsax by Associate II
  • 7804 Views
  • 22 replies
  • 0 kudos

STM32F407VG ( F4 discovery board) I2C issue

Posted on May 12, 2014 at 00:20 Hi guys, i have a problem regarding comunicating with a sensor via i2c. This is my first atempt to use i2c comunication on a ARM piece My code for the sake of time saving is this one bellow( original f...

Bogdan by Senior
  • 3256 Views
  • 8 replies
  • 0 kudos

USART Interrupt triggered too often

Posted on May 15, 2014 at 13:44 I'm using USART with circular buffers and interrupts to transmit and receive. To transmit, a byte is written to the buffer, the TXE interrupt is enabled and then the byte is sent and theTXE Flag is cleared in t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.