2014-05-16 4:37 AM
Hi,
My RTC (F103) is currently running from LSI. The counter is counting properly, and the SEC flag in CRL is set every second as expected. When the Alarm is set, the SEC flag is asserted and cannot be cleared anymore. Also the alarm flag never gets set regardless of the value written to the ALRL and H registers. Here's an example: withRTC_SetAlarm line commented, the led changes it's state once every second.
RTC_ClearFlag(RTC_FLAG_SEC);
while(RTC_GetFlagStatus(RTC_FLAG_SEC)==RESET);
//RTC_SetAlarm(RTC_GetCounter()+10);
RTC->CRL = 0;
while (1)
{
x = RTC_GetFlagStatus(RTC_FLAG_SEC);
if (x)
{
BRD_LedToggle(LD2);
RTC_ClearFlag(RTC_FLAG_SEC);
RTC->CRL = 0;
}
}
Uncommenting the
RTC_SetAlarm(RTC_GetCounter()+10) results in always true if condition that blinks the led on every iteration of the while loop. Clear flag does nothing and the flag is constantly asserted.
Can anyone replicate this problem? What would be the source of it?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.