STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard fault problem

Posted on June 10, 2014 at 16:34 For several years I have developed software for an STM32F103 target using Eclipse/OpenOCD/Olimex ARM-USB-OCD. Recently my hard drive failed so I replaced it and re-installed everything. My project will not now ru...

DMA into GPIO peripherial

Posted on June 10, 2014 at 16:54Hi all, I have a project where I need to deal with 4-to-8 bit and 8-to-4 bit conversion and so I have a questions: 1. I know that I can do DMA to/from GPIO but what is maximum speed of that operation. Can I go up to 2...

pawwodko by Associate II
  • 1826 Views
  • 3 replies
  • 0 kudos

Problem with STM32F103ZE SPI data send

Posted on June 04, 2014 at 04:47Hello I am trying to send opcode bytes MCBSTM32 to GP22. But as I debug in Keil I observe the the byte to be sent(0x50) is nit being written on the SPI data register in stm32f10x_spi.c. Instead the data register is sh...

CPU,DMA UART Transfer Independently

Posted on June 05, 2014 at 22:21Hello,       I want to transmit 10000 samples taken by adc continuously stored in an array. Is it possible the DMA-UART can transmit this to the PC while the CPU can take the next set of samples(independently) i.e wit...

Upload A Binary File In Web Server

Posted on June 07, 2014 at 16:46Dear all, If someone can solve my problem : I'm working on STM3221G-EVAL Board .. I want to know how can I upload a Binary File in a web server ... Thanks

CHN1 and CHN1N collision - is it posible ?

Posted on June 07, 2014 at 16:52 hello dear forum I designed an inverter for vibration tank ( photo below ) it issimply an H bridge with 500 V 20 A mosfets the frequency and duty is variable with STM32F103 the vibrator worked...

0690X00000602v8QAA.jpg

Alternative usage of timer channel pins

Posted on June 10, 2014 at 15:42Hello, as described in the reference manual, the STM32F103 have timers with up to four channels - for example TIM1 - TIM5. But in my application i need only one channel (for output compare or pwm output). In the Micro...

STM32F103RC SPI3 configuration

Posted on January 14, 2014 at 09:16Hello,I can't get SPI3 on pins (PB3, PB4. PB5) working. On the scope I checked that SPI clock is running. But still I can't read MX25L6406E flash ID. Functions that handles flash commands are checked and is working...

linas by Associate
  • 2162 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.