STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 - FLASH Erase

Posted on December 11, 2013 at 20:54I am attempting to erase a FLASH sector, but the process hangs. Any ideas on why this might be happening?    FLASH_Unlock();    FLASH_ClearFlag(FLASH_FLAG_EOP | FLASH_FLAG_OPERR |                 FLASH_FLAG_WRPER...

dibs by Associate II
  • 6729 Views
  • 12 replies
  • 0 kudos

Migrating from STM32F2 to STM32F4

Posted on June 11, 2014 at 10:58Hello,I can't found a guideline for migrating from STM32F2 (207) to STM32F4 (429) on st.com. I find only STM32F1 to F2 or F4Has anyone docs or note about it? Or some reference to doc...Are there any different between ...

kruzicka by Associate II
  • 2322 Views
  • 4 replies
  • 0 kudos

STM32F2xx SPI DMA FIFO error

Posted on September 25, 2012 at 00:36When I use DMA on the transmit SPI2 chanel (STM32F205) I consistently get FIFO errors at the end of the transfer, even though the FIFO is disabled.  I verified the DMDIS flag is 0 in the DMA_SxFCR register but th...

SPI transfer problem

Posted on June 10, 2014 at 22:51 Hi all; I'm trying to make two boards communicating with SPI. The Master is a board based on PIC µC and the slave is Discovery F3. The protocol that i have to establish is as follows: 1) The master...

khalid2 by Associate II
  • 950 Views
  • 1 replies
  • 0 kudos

STM32-Mat TIMx-IRQHandler multiply defined

Posted on June 11, 2014 at 11:53Trying to generate a simple PWM Output using STM32-Mat Timers 1 and 8 work flawlessly, however the other available timers (2,3,4,5) all produce error 6200: TIMx-IRQHandler multiply defined by stm32f4xx.o and PWMTest.o...

marc2 by Associate II
  • 812 Views
  • 0 replies
  • 0 kudos

Lwip stack for Standalone STM32F407VG

Posted on June 06, 2014 at 15:42Hi AlI have referred to  AN3966 (LwIP TCP/IP stack demonstration for STM32F407/STM32F417 microcontrollers) to get LWIP stack for Standalone STM32F407VG. And also i got LWIP stack files from a link http://www.st.com/we...

ecmanja by Associate II
  • 4871 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.