2014-06-07 7:46 AM
Dear all,
If someone can solve my problem : I'm working on STM3221G-EVAL Board .. I want to know how can I upload a Binary File in a web server ... Thanks2014-06-07 8:06 AM
Not sure exactly what you're asking, you want to have a web server, and want to send it a file?
What software/protocol do you want to be using to do this? You want the web server to serve up arbitrary binary files you supply, perhaps stored on an SDCard?[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/HTTP%20Server.%20Webpage%20in%20SD&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=235]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FHTTP%20Server.%20Webpage%20in%20SD&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=2352014-06-07 9:14 AM
Thanks for your help, clive1.
Yeah! this is what i wanted : -I want the
web
server
to serve
arbitrary binary
files provided
, stored on
an SD card
? But first, Could you tell me how can I implement an http server using the lwip v1.1.0 stack on STM3221G-EVAL board and how to send it a file... .. Thanks2014-06-07 12:45 PM
Take STM32F2x7_ETH_LwIP_V1.0.2\Project\FreeRTOS\httpserver_socket\src\httpserver-socket.c, or current equivalent. This supports hard coded files which are compiled into the image.
You need to add SDIO code, along with the FatFs file system. You can write to the card on a PC, or alternatively you could create a USB MSC and access it like a flash drive. In the other thread I showed how the file serving routines could be modified to pull data from the SD Card instead of the compiled file image. I ported it to ,2014-06-09 3:21 AM
the task is
really complicated
..
and
the countdown
is triggered
for the filing
of
project
...
Pleaseyou can
give me
the steps
again
one by one
...
From
the configuration of the
boards
until the
file sent
by the web server...
Thanks.2014-06-09 3:44 AM
Just for information :
I'm not using an RTOS but a standalone mode. In this mode, the ethernet system provides very poor functionality.2014-06-09 7:19 AM
May be those are things you need to discuss with your project supervisor.
As I have suggested, break the problem into smaller tasks you can solve. Test the SDIO implementation, put a file system on top, get comfortable with opening and accessing files. STM32F2xx_StdPeriph_Lib_V1.1.0\Project\STM32F2xx_StdPeriph_Examples\SDIO\uSDCard STM32F2xx_StdPeriph_Lib_V1.1.0\Utilities\STM32_EVAL\STM322xG_EVAL\stm322xg_eval_sdio_sd.c STM32F2x7_ETH_LwIP_V1.1.0\Utilities\Third_Party\FatFs_vR0.08a STM32F2x7_ETH_LwIP_V1.1.0\Project\Standalone\httpserver Consider using the RTOS, it might make things easier, otherwise you'll need to work the server code to find the correct place/method to support files from the SDCard via FatFs2014-06-10 3:47 AM
Hi clive,
Please Can
yougive me
some
informations
about
the
connection between
the
STM32
BOARDS
pc
and router
.. Thanks.2014-06-10 10:08 AM
To connect a node device to a hub/switch you use standard CAT5 ethernet cables with a one-to-one connectivity.
To connect two node devices (PC, STM32, etc) to each other you need a cross-over cable which switches the TX and RX pairs. Generally when developing 100BT Ethernet systems you should use a router which can provide IP addresses via DHCP, and you allocate a unique MAC address to all you attached devices. If you route signals through a HUB (10BT?), all input signals will be reflected on all other ports, you could connect a PC running WireShark to one port to observe all traffic. HUB != SWITCHWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.