STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Encoder mode - Prescaler or external trigger filter

Posted on August 21, 2014 at 14:46Hi everyone, I've been working on the STM32F4 and I would like to count pulses from some odometer. There are two types of odometer, the ones that output two signal in quadrature and the other that output pulse on ...

maxime2 by Associate
  • 1154 Views
  • 1 replies
  • 0 kudos

PID PROBLEM IN CONTROLLER STM 32

Posted on August 21, 2014 at 10:02Hi,i am facing problem for the PiD controller.what parameter i have to use it for the positive & negative nos for calculation purpose.Kindly look following code New_Duty_cycle_buck=(Previous_Duty_cycle_buck + Error_...

deepak by Associate II
  • 1240 Views
  • 2 replies
  • 0 kudos

synchronous USART

Posted on August 19, 2014 at 16:38Hi everyone.I need to build a system based at STM32F4xx that use absolute encoder with BiSS protocol (http://www.biss-interface.com). This protocol is based at synchronous RS485. I have HW that convert differential ...

0690X00000602t3QAA.jpg
artuom by Associate II
  • 1626 Views
  • 2 replies
  • 0 kudos

STM32L152C6 LSE RTC WakeUp

Posted on August 26, 2013 at 09:49 Hello. I'm trying to use the RTC WakeUp feature to as a countdown timer. I've tried the code from the StdLib examples: void RTC_Config( void ) { NVIC_InitTypeDef NVIC_InitStructure; EXTI_Ini...

kaloyan by Associate III
  • 2375 Views
  • 4 replies
  • 0 kudos

STM32F407 TIM2_CH1_ETR

Posted on August 20, 2014 at 20:00Maybe this is explained somewhere in the RM, but because I didn't find the answer with a brief study I will try if the forum can help... So the question is about the alternate function pin named TIM2_CH1_ETR. I want...

ari239955 by Associate II
  • 3283 Views
  • 3 replies
  • 0 kudos

PWMInput problem

Posted on August 19, 2014 at 02:26 Hi, I am trying to get the signal from a RC receiver (typical servo's signal) but i am not getting any reads even though the timer interrupt is working. PWMI - PB10 -CH3 Signal: 50 HZ (Duty ...

jdpv by Associate II
  • 1558 Views
  • 5 replies
  • 0 kudos

Uart vs Usart on DMA

Posted on August 20, 2014 at 18:25Hi, I'm complete noob with STM32 but starting to get the hang of things. I have problem that got me completly stumped now.  I have simple code that sends string over Uart4 . When using polling or _IT the string is ...

GPIO interrupt change other pin state

Posted on August 20, 2014 at 11:54 Hello, i am facing strange problem with STM32F4 I have +-10V power supply that is enabled with GPIOB Pin 2. When i start program, it will enable power supply, just like i declare in startup; GPIO_SetBits(GP...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.