cancel
Showing results for 
Search instead for 
Did you mean: 

LCD_DisplayStringLine(Line5, ''Hello'');

jeu
Associate II
Posted on August 18, 2014 at 15:44

Where can I find the definition of LINE(5)? I would appreciate for it. Jai

Please note that:

&sharpdefine Line5 LCD_LINE_5  at stm32_eval.h

&sharpdefine LCD_LINE_5 LINE(5) at stm3210c_eval_lcd.h

#lmgtfy #stm32f10c-eval
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Andrew Neil
Super User
Posted on August 18, 2014 at 16:30

#define Line5 LCD_LINE_5  at stm32_eval.h

 

#define LCD_LINE_5 LINE(5) at stm3210c_eval_lcd.h

If you can work back through those two defines, why can't you take the next step back to the definition of LINE ?

What toolset are you using -doesn't it have -'go to definition'?

Or just grep ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
jeu
Associate II
Posted on August 19, 2014 at 03:19

Hello Neil,

CoIDE is used. When LINE(5), for example, is not searched any further. It looks like a micro that determines (x,y) cordinates. Unfortunately, I cannot find out the data sheet of 3.2'' TFT LCD used in STM32107C_EVAL kit.

Jai

Posted on August 19, 2014 at 06:17

2.4''

http://wenku.baidu.com/view/9199760dba1aa8114431d94b.html

3.2''

http://gamma.spb.ru/media/pdf/tft-displei/AM-240320D4TOQW-T00H%28R%29.pdf

ILI9320

http://www.densitron.com/uploadedFiles/Displays/Support/ILI9320DS_V0.51.pdf

STM32F10x_StdPeriph_Lib_V3.5.0\Utilities\STM32_EVAL\Common\fonts.h

#define LINE(x) ((x) * (((sFONT *)LCD_GetFont())->Height))

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
Posted on August 19, 2014 at 09:08

''CoIDE is used. When LINE(5), for example, is not searched any further''

You need to raise a bug report with CooCox, then.

''It looks like a micro''

*m

a

cro

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
jeu
Associate II
Posted on August 20, 2014 at 10:22

Hello Clive1,

Thank you very much for PDF files and LIVE macro. Now I see the printout on the screen. However, each line printout is flipped around x axis (right to left, mirror image). I wonder if there is another setting along with this.

Thanks again.

Jai

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.