STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN Baud rate

Posted on February 20, 2012 at 04:11 Im trying to use the CAN interface on the STM32F4 discovery board. I am using the STM code sample which says it configures it to 1Mbit baud rate but this doesnt seem to be the case, with an oscilloscope hooke...

pisaacs9 by Associate II
  • 6991 Views
  • 12 replies
  • 1 kudos

Controller to read wav files from SD CARD

Posted on August 19, 2014 at 15:45I need a little help to choose the right device.I would build a digital audio player with the following characteristics:  - it should read data from SD card only (up to 32GB size)  - SD card will be formatted FAT32 ...

[SOLVED]Proper clock initialization for STM32F401RB

Posted on August 23, 2014 at 09:52 Hi, I am using a custom board withSTM32F401RB MCU and I want to run it at 84MHz from PLL<-HSE configuration. I have an 8MHz crystal on the board. But I don't know how to do it. I ran the STM32CubeMX (I don't...

petoknm by Associate II
  • 1333 Views
  • 0 replies
  • 0 kudos

Undefined symbol error - no compile

Posted on August 22, 2014 at 06:05Hello, I load several example projects unmodified into Keil and compile as soon as I enter. When the project enters the linking phase, I get an error that HAL_DMA_Init is an undefined symbol, and the project won't c...

david2399 by Associate II
  • 1995 Views
  • 2 replies
  • 0 kudos

pwm output timer1

Posted on July 06, 2014 at 15:59 hi guys, i create a program to generate pwm signals in stm32f407 i did it in past for another timer but when i wanna do it for timer1 i doesn.t work. here is my code : #include <stm32f4xx.h> voi...

CAN message

Posted on August 21, 2014 at 20:08Hi, I am trying to use CANbus on STM32F303VC6. I get it working in loopback mode. But the message is not getting sent in Normal mode. I have turned on SB21 and SB22 to connect the ports PA11 and PA12 to P2. When I d...

rizwin by Associate II
  • 1466 Views
  • 3 replies
  • 0 kudos

Sharing PA5 between HS USB and DAC2 on STM32F4

Posted on August 16, 2014 at 06:06HiI have problem in sharing the PA5 functionality on STM32f407IGT6.As I need to use both of DACs in my design, and HS_ULPI_CK is also routed only on that pin (there is no multiplex to any other pins).I can not use O...

sbsohrabi by Associate II
  • 2282 Views
  • 5 replies
  • 0 kudos

STM32F429 Discovery SPI Registers

Posted on August 21, 2014 at 16:14 I am trying to use theSTM32F429 Discovery boardin order to communicate in a transmit only mode to an LCD over SPI. However, every time I write to the data register to output, I see nothing get loaded in my debug...

cns1307 by Associate II
  • 1382 Views
  • 6 replies
  • 0 kudos

Can TIM16 & TIM17 be used in external clock source mode1?

Posted on September 04, 2013 at 18:42Hi, I would like to know if TIM16 and TIM17 can be used in external clock source mode 1. There is any reference in the Reference Manual that it doesn't. So I suppose it is possible. I develop my board and now I w...

tecnico23 by Associate II
  • 1076 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.