STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407, Timer6 running 2x too fast (SOLVED)

Posted on September 12, 2014 at 09:12I'm reluctant to post this because I figure it's operator error, but I'm stuck.  I'm running an STM32F407 Discovery board using AdaCore's Ada2012 release.  Simple tasks seem to run correctly, and at the correct s...

kk6gm by Associate II
  • 1210 Views
  • 2 replies
  • 0 kudos

Scale SPI1 clock to 10kHz in STM32 discovery

Posted on September 11, 2014 at 14:52Hello all,I am trying to establish SPI communication bw STM32FDiscovery board and MCP3202 ADC. The optimum clock rate of MCP3202 is given as 10kHz in the datasheet. I am using SYSCLK as 48MHz in my Discovery boar...

sandhya by Associate II
  • 1530 Views
  • 2 replies
  • 0 kudos

FSMC WR behavior

Posted on September 12, 2014 at 12:47In a nearly ready project i wanted to add some more types of TFT displays. Now i�ve got one with an SSD1298 controller, for which well working init-code is available. I connected it in well known manner to the FS...

ralf2 by Associate II
  • 652 Views
  • 0 replies
  • 0 kudos

Lwip stm32cubeMX FW_F4_1.3.0 bug

Posted on September 11, 2014 at 19:54Hi, I'm using an olimex stm32e407 board. I select the option lwip but with FW_F4_1.3.0 dont work, ping without success. But if i select in the stm32cubeMX the FW_F4_1.1.0 the ping work. I don't understand why. R...

ADC and DAC Issues with STM32F4VGT6

Posted on September 11, 2014 at 17:30 Hi, I am using trying to use the ADCs on the STM32f4vgt6 with the DMA Controller in continuous conversion mode. I have this chip mounted on a custom board and I am using 8 ADC channels. Below is my in...

k2399 by Associate
  • 1706 Views
  • 3 replies
  • 0 kudos

SPI1 Almost working but no MOSI?

Posted on September 11, 2014 at 19:35 I'm trying to get SPI1 up and running with STM32F4 as a master. This was the source code / tutorial. The only changes are: MOSI is on pin PB5 instead of PA6 in the example and CS is on PA4 instead of P...

boris2 by Associate II
  • 1463 Views
  • 1 replies
  • 0 kudos

STM32 ADC multiple channel use

Posted on August 27, 2014 at 18:41To get data from multiple channels for any ADC, what function should i use?For egIf i configure my ADC with the following : ADC_RegularChannelConfig(ADC1,ADC_Channel_0, 1,ADC_SampleTime_1Cycles5);ADC_RegularChannelC...

spuri by Associate
  • 1553 Views
  • 2 replies
  • 0 kudos

ST-Link on Windows8 64bit

Posted on April 01, 2013 at 12:21I have installed Windows 8  Pro K on my PC.0I can't install your up-to-date ST-Link driver.And I tried several times as your suggestion like below, but I have failed all./public/STe2ecommunities/mcu/Lists/cortex_mx_s...

mhlee by Associate
  • 1989 Views
  • 4 replies
  • 0 kudos

Can't get data from UART

Posted on September 10, 2014 at 00:13I'm trying to get data from the usart by waiting for RXNE to get set, but somehow it doesn't ever happen, and it gets stuck forever waiting. An equivalent program on PC communicates just fine with the same endpoi...

jaravena by Associate
  • 3072 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.