STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDD1963 LCD Controller with FSMC

Posted on March 11, 2013 at 20:21Hello, Does anybody already used sdd1963 lcd controller with STM32 through FSMC? The used code to configure the FSMC is: void FSMC_LCD_Init(void) {   FSMC_NORSRAMInitTypeDef  FSMC_NORSRAMInitStructure;   FSMC_NORSRAM...

gsilva by Associate II
  • 2515 Views
  • 4 replies
  • 0 kudos

STM32L0 MCU EEPROM write

Posted on July 29, 2014 at 14:44Hi.I use Nucleo board with STM32L0x3 MCU. There are special sequence for EEPROM TYPEPROGRAM_BYTE process? I can write 4 bytes data (TYPEPROGRAM_WORD) but can't write 1 byte data (TYPEPROGRAM_BYTE):uint32_t Address = 0...

STM32F205 flash self programming

Posted on September 06, 2014 at 22:11Hello, First, sorry for my poor english.I have a problem with a STM32F205. I am trying to read the content of flash memory , and for some bytes i have a value different with my firmware binary file. But the appli...

msstaf by Associate
  • 1374 Views
  • 2 replies
  • 0 kudos

What is the default PriorityGroup setting if I didn't call NVIC_SetPriorityGrouping or NVIC_PriorityGroupConfig

Posted on September 13, 2014 at 22:14I'v found in the Cortex-M4 file that the default value of PRIGROUP is 0. while the legal value of STM32 is from 3 to 7. And I didn't find the PRIGROUP set in startup file or system_stm32f4xx.c. What is the defaul...

STM32L0x ISP though USART

Posted on September 12, 2014 at 11:22Can anybody point me to the software for programming STM32L0 family through USART bootloader? Flash loader demonstrator doesn`t seem to support this family.Thanks in advance #stm32l0-isp-bootloader

Failed to configure the system clock for STM32F103

Posted on September 13, 2014 at 01:12 Hi, I am trying to create a 64MHz system clock by using the 8MHz HSI clock and the PLL (PLLMUL = 16). But the firmware stops working after this line: RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);...

STM32 crashed during programming flash

Posted on September 12, 2014 at 13:43Hi, My project crashed during programming of STM32L152 internal flash. Crashing means, that I cannot halt CPU; no hard fault nor bus fault interrupt only CPU freezed. Project runs CMSIS-RTX RTOS. Program is runni...

zoltan2 by Associate II
  • 1564 Views
  • 2 replies
  • 0 kudos

SysTick interrupt problem

Posted on September 05, 2014 at 19:12 hi every body . i have systick in 25hz(each 0.04 sec) send my sensors data through usart. but the it just execute my main ''while(1)'' just once , and after that just my void SysTick_Handler(voi...

STM32L0 flash loader support

Posted on September 11, 2014 at 20:01Am I missing something or flash loader demonstrator 2.6 doesn`t support STM32L0x devices?Seems that there is no appropriate *.map file for that family. #stm32l0-flash-loader-demonstrato

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.