2014-09-12 3:47 AM
In a nearly ready project i wanted to add some more types of TFT displays. Now i�ve got one with an SSD1298 controller, for which well working init-code is available. I connected it in well known manner to the FSMC and it happened NOTHING...Studying the documantation of the display in precision i see: WR ist Write signal, active at Rising edge !!! So my problem is that the FSMC provides an active low Signal. Is it possible to change this behavior? I would not like to put additional hardware to the ready project. Has someone an idea? Thanks
#fsmc-stm32-wr-lineWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.