STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Digital Photo Frame

Posted on November 28, 2014 at 14:22An STM32F103 Based Digital Photo Frame utilizing uCGUI Graphics Framework with source code. This is a good tutorial if you want to learn using Graphics Framework uCGUI from Micrum, FAT FS Embedded File System by C...

What is CPRI on the HD STM32L1?

Posted on November 26, 2014 at 18:05Hello, looking at the datasheet of the HD STM32L1 devices, A CPRI function is listed in table 10. However I didn't find any information on the web and on the ST website about that function. Any information welcome...

STM32F407VG Eval Board

Posted on November 27, 2014 at 14:02Hi,                    I am a beginner in the ARM Cortex Series and so far I could able to run some simple examples on my STM32F407VG Board. Currently I am working with a project where I need to establish the comm...

jayakanth by Associate II
  • 2319 Views
  • 5 replies
  • 0 kudos

Delete (mass erase) flash bank 2 on STM32F429II

Posted on November 27, 2014 at 14:06 I have a STM32F429II with 2 x 1MB flash memories. It supports Read-While-Write on the flash banks. I have written code to write/read to the flash memory bank 2 and my application is on the flash bank 1. I hav...

phb by Associate II
  • 1658 Views
  • 1 replies
  • 0 kudos

STM32F303RE: linker file for GNU based tool chain

Posted on October 17, 2014 at 17:05Hi,I have a c++ application that is running on STM32F303RC (256 K flash).I want to use this same application on the new STM32F303RE (512 K flash).I modify the linker file as follow:/* Entry Point */ENTRY(Reset_Hand...

[solved] works FSMC correct on stm32f407vg ?

Posted on November 25, 2014 at 11:33 Hi. All! I want to use FSMC module, but I'm not sure that it settings correct. There is write operation on a picture. I see multiple NWE activation. And sometime it release NEx together NWE (should be NWE...

0690X00000602yqQAA.jpg
t2399 by Associate II
  • 5286 Views
  • 8 replies
  • 0 kudos

TEC CAN error instantly full

Posted on November 27, 2014 at 20:31Hi all!   In what cases will the Transmit Error Counter register jump from 0 to 0xF8? I am debugging this CAN transmission sequence, and after the Transmit request is set, the next step in debug will show a full E...

zamolan by Associate II
  • 1270 Views
  • 0 replies
  • 0 kudos

Run code from SDRAM with STM32F4 (e.g. STM32F229)

Posted on November 18, 2014 at 14:14Hello, we are considering to use the STM32F4, probably the STM32F429 or STM32F427. For our application we would need to run the program from SDRAM. I was looking around for application notes, but could not find s...

stcom9 by Associate II
  • 6851 Views
  • 13 replies
  • 0 kudos

Compilation with files from STM32CubeF4 on linux

Posted on September 06, 2014 at 09:02Hello all. I just got a STM32F429-DISCO board and compiled my first successful program. I'm working under linux compiling with the GNU toolchain for ARM. In order to be able to compile my program, I had to modify...

pgarista by Associate
  • 1290 Views
  • 3 replies
  • 0 kudos

STM32F4 timer (Prescaler Value)

Posted on January 24, 2013 at 03:46Hi, I have just saw a program about a interrupt time. The program can let the LED on and off in a specified period. But I have some question about the prescaler value, can anyone help me to understand the prescale ...

kazafwing by Associate II
  • 6438 Views
  • 13 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.