2014-11-27 11:31 AM
Hi all!
In what cases will the Transmit Error Counter register jump from 0 to 0xF8? I am debugging this CAN transmission sequence, and after the Transmit request is set, the next step in debug will show a full ESR : 0x00F80057. Is this meaning an incomplete configuration of CAN module and GPIO Pin? Or a nonfunctional CAN Transceiver? I would be more than happy if you can give me a hint on it. I have attached the registerlayout screenshot of the CAN1 module after the debugger left the CANTransmit() function. #can #tec-registerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.