STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Conversion

Posted on November 30, 2014 at 23:44I'm currently working on a university project that involves the analogue to digital converter on the STM32F0 discovery board. I've studied the manual and (as far as I can tell), initialized the registers correctly...

eric23 by Associate
  • 1021 Views
  • 1 replies
  • 0 kudos

clear USART TC flag

Posted on November 27, 2014 at 21:20Hi I am using USART in Interrupt mode in Tx and Rx. Rx is working fine But in Tx I keep getting interrupt. I just need to get the interrupt once when the data is sent. but I keep getting the interrupt again and ag...

hossam by Associate II
  • 4661 Views
  • 5 replies
  • 0 kudos

dead time in stm32f4

Posted on November 29, 2014 at 17:24I'm generating a 50Hz complementary PWM wave in stm32f4 i'm stuck on dead-time insertion as i want to insert a dead time of 2.5ms, I don't know how to do that here is my code. This is what I thought it should be b...

Which USB mode for high speed transfer?

Posted on November 29, 2014 at 04:36Hi, I've been working with the STM32 for several years, but never done any USB related stuff. Just recently I've got working an example of USB-HS using the mass storage class.In my application I have a 16Gbyte SD ...

carl2399 by Associate III
  • 2863 Views
  • 4 replies
  • 0 kudos

Cortex M3 bit banding

Posted on November 23, 2014 at 13:35Dear All, I red the ARM reference manuals regarding  the ''bit banding'' to understand the operation.   I do not understand how it's overcome the RMW (Read modify write )behaviorlease adviceThanks in advance

pic_micro by Associate II
  • 2841 Views
  • 6 replies
  • 0 kudos

Code works differently in debug mode than in real time

Posted on November 26, 2014 at 23:47 Hello. I've got problem regarding STM32L100 (on discovery board). I've switched from Arduino where I enjoy the simplicity of printing data to via UART and delay/millis functions. So, I decided to write my own...

How are you supposed to use HAL_UART_Receive in STM32Cube ?

Posted on November 25, 2014 at 18:52I am implementing a command parser that receives data on a serial port. My need is to read one byte at a time and when I recive a full command I will handle it. I look at the example in STM32Cube_FW_L0_V1.1.0\Proj...

johan2 by Associate II
  • 2013 Views
  • 2 replies
  • 0 kudos

TIM_ICPOLARITY_BOTHEDGE Input capture in STM32L

Posted on November 28, 2014 at 19:24Hello Guys,I´m developing an application with STM32L and I would like to use TIM2 Input capture with TIM_ICPOLARITY_BOTHEDGE.When the interrupt occurs...Is there a way of knowing which Polarity has been detected?M...

gerardo by Associate II
  • 3077 Views
  • 7 replies
  • 0 kudos

can t compile ARM_MATH.h

Posted on November 27, 2014 at 21:35Hi, I am using coide and arm gcc compiler to build my projects.When i try to compile arm_math.h ,i got those  errors a LOT of times.unknown type name '__INLINE expected '=', ',', ';', 'asm' or '__attribute__' befo...

d4ng3r09 by Associate II
  • 1223 Views
  • 3 replies
  • 0 kudos

DAC waveform generation with DMA not working

Posted on November 27, 2014 at 15:45I am using the STM32L Discovery Board (STML152RB chip on board). The IDE is Emblocks. I was trying to generate a sawtooth wave signal using DAC and DMA but it does not work. I was able to make the same program wit...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.