STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F437 video compression H264

Posted on December 02, 2014 at 11:44Hello. In a project we are developing we use the STM32F437 MCU for streaming video. What I would like to know is if with the 256KB RAM it has, it is enough for compress the video in H264. We have not free size to ...

javier by Associate
  • 3246 Views
  • 2 replies
  • 0 kudos

I2C execution speed, with vs without DMA using HAL driver

Posted on December 01, 2014 at 12:56Hello, I am interfacing SC620 LED driver using I2C. Here is a function where writing to the LED driver occurs./** * Write data to SC620 led driver register. * * @param[in] reg      Select register. * @param[in] va...

primozic by Associate II
  • 3974 Views
  • 8 replies
  • 0 kudos

Improve bitbang driver speed

Posted on November 24, 2014 at 21:06Hi,I am using the STM32F2xx cube API to implement a raw bitbang usb driver for the FTDI ft245.  I am currently achieving speed of 5000 bytes/s.  I would like to improve the speed.  The bitbang code is simple as:<....

ST-Link upgrade

Posted on December 01, 2014 at 15:56I am using stm32fvldiscovery card and Kiel uv4. Flash download fails with dll fail messages ( these are different today to yesterday) But when I ran a kiel provided STlinkupgrade.exe it reported old firmware versi...

CAN on stm32f303xC processor

Posted on November 21, 2014 at 14:58The original post was too long to process during our migration. Please click on the attachment to read the original post.

ADC Help Needed

Posted on November 30, 2014 at 23:45I'm currently working on a university project that involves the analogue to digital converter on the STM32F0 discovery board. I've studied the manual and (as far as I can tell), initialized the registers correctly...

eric23 by Associate
  • 1244 Views
  • 3 replies
  • 0 kudos

USB: how to manage disconnect and re-connect the cable

Posted on December 01, 2014 at 09:48Hello all,my application is based on stm32l152, I use StdPeriph_Driver and STM32_USB-FS-Device_Driver.USB transfer works fine until I disconnect usb cable. After disconnecting the firmware stuck running just inter...

bruzzim by Associate II
  • 2086 Views
  • 2 replies
  • 0 kudos

STM32L100 ADC Result Error On wakeup from Stop Mode

Posted on November 24, 2014 at 10:56Hi,    My application wakes-up from Stop Mode every 100mSec, takes ADC conversion from two channels in Scan mode to DMA then makes some processing. I get roughly +1.5% error. When i disable the Stop Mode but sampl...

aboyarski by Associate II
  • 1660 Views
  • 3 replies
  • 0 kudos

RTC GET_TIME / SET_TIME STM32-F4 DISCOVERY BOARD

Posted on November 07, 2014 at 10:22hello all ,does any one have a working code example  for keil  for RTC / calander ...for get or set time and date ( i need it to home automation system) thanks in advanced.(i don't conect 32k ... external crystal)...

maor by Associate III
  • 1512 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.