STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F2 VCP Tx Handling USBD_BUSY

Posted on November 26, 2014 at 02:47I am using VCP firmware from STM, but I have a problem when I am transmitting my data using the CDC classI am sending data from my firmware to my PC, if I did open the serial port in my PC side, and i am still sen...

hosweetim by Associate II
  • 3347 Views
  • 5 replies
  • 0 kudos

STM32F030 Eval Board PORTF.0 Problem

Posted on December 03, 2014 at 05:33I am using an �030 with its internal oscillator.  Thus I should be able to use F0 and F1 for anything any GPIO pin can be used for.  I turned on internal pullups on these pins and only F1 worked.  F0 read high or ...

picguy2 by Associate II
  • 729 Views
  • 0 replies
  • 0 kudos

STM32F4 output compare toggle - how to set initial state

Posted on December 02, 2014 at 08:29Hello ! I am struggling to set the initial state from which the toggle mode of output compare (STM32F405, TIM1) starts. I tried to set OCM1 mode to '101 : force active level', '100 : force inactive level' respecti...

kilian by Associate
  • 1227 Views
  • 2 replies
  • 0 kudos

USB: how to increase the input and output receive buffer

Posted on December 02, 2014 at 21:24Hello,I designed my own application starting from VirtualComport_loopback example project.I have a modbus client protocol running on USB and using CDC_Send_DATA() and CDC_Receive_DATA() send and get data from PC v...

bruzzim by Associate II
  • 683 Views
  • 0 replies
  • 0 kudos

Vbat Current

Posted on November 07, 2014 at 17:52I am working with a STM32F051xx for a real time clock application. Looking at the datasheet (page 53, table28: typical and maximum current consumption from the Vbat supply), it is noted below the table that the MC...

dave23 by Associate II
  • 3851 Views
  • 2 replies
  • 0 kudos

FatFs examples

Posted on December 02, 2014 at 18:43hi every oneim trying to use FATFS file system library for stm32f103 with keil 5.12 & mmc cardkeil show some errors like : error:  #20: identifier ''asm'' is undefinedhave any one a example of FAT FS for stm32f103...

mhdizgah by Associate II
  • 808 Views
  • 0 replies
  • 0 kudos

Problem with ADC interruptsin continuous mode

Posted on November 30, 2014 at 20:08 Hi , I have a problem in the program after enabling the ADC interrupt , The processor doesn't do anything after starting ADC_READ Here is a simple program which reads data from ADC in continuous mode and w...

TCP/UDP Echo Server Example

Posted on March 19, 2012 at 18:21Hello, did anybody try the TCP/UDP echo example from stm32f2x7_eth_lwip.zip? It compiles out of the box, and tcp echo works fine if tried first, but udp echo does not work for me (I am using a STM32F220G-EVAL board)....

zabel by Associate III
  • 4385 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.