2014-11-30 2:45 PM
I'm currently working on a university project that involves the analogue to digital converter on the STM32F0 discovery board. I've studied the manual and (as far as I can tell), initialized the registers correctly, but no conversion is happening. Would anyone be able to point out flaws in my code or logic? This is all fairly new to me, so I might be missing something obvious.
int main(int argc, char* argv[]) { // Clock signals RCC->AHBENR |= RCC_AHBENR_GPIOAEN; myADC_Init(); while(running == 1) { uint16_t adcOutput = ADC1->DR; trace_printf(''%d'', adcOutput); } } return 0; } void myADC_Init() { // Set PA2 to analog mode // PA2 will serve as input to the ADC GPIOA->MODER |= GPIO_MODER_MODER2; //Enable the ADC Clock RCC->APB2ENR = RCC_APB2ENR_ADC1EN; //Calibrate the ADC ADC1->CR |= ADC_CR_ADCAL; //Wait until calibration is complete while(ADC1->CR & ADC_CR_ADCAL); //Turn on the ADC ADC1->CR |= ADC_CR_ADEN; //Wait until the ADC is ready while(!(ADC1->ISR & ADC_ISR_ADRDY)); // Ensure that the ready flag has been triggered in the ISR //ADC1->ISR = ADC_ISR_ADRDY; // ADC continuous mode (1 in bit 13) ADC1->CFGR1 = ADC_CFGR1_CONT; ADC1->CFGR1 = ADC_CFGR1_OVRMOD; // Channel 2 selected for conversion ADC1->CHSELR = ADC_CHSELR_CHSEL2; // Sampling time is 239.5 ADC clock cycles ADC1->SMPR |= 0x7; ADC1->CR |= ADC_CR_ADSTART; } I've connected a 3.3 V square wave to PA2 of the board, and confirmed this wave with an oscilloscope. My understanding is that, because the ADC is set to obtain input from PA2, it should automatically convert data connected to that pin? I've been printing the ADC data register values, and I only ever get 0. Obviously something is going wrong here. Any help is appreciated! #adc-help2014-11-30 4:37 PM
Perhaps you're not ready for register level coding, try looking at the examples posted on the forum, and using the standard peripheral library.
2014-11-30 7:10 PM
Well it wouldn't matter if I'm not ready. I've been assigned a project and I plan on completing it. As for whether I'm ready, of course I am. Why wouldn't I be? I understand the material just fine. If all programmers gave up because of small bugs in their code on the first attempt, nobody would learn anything.
Anyways, as per the project specifications, I can't use the library. Only registers are allowed. I did get it working. The board I was using wasn't working properly. I switched to another board in the lab and the ADC works fine.2014-12-01 9:54 AM
If all programmers gave up because of small bugs in their code on the first attempt, nobody would learn anything.
Nobody asked you to give up, just suggested looking at the problem from a different perspective, allowing you to compare how the register configuration differs between the two. It would provide an expeditious way to sanity check the hardware, regardless of whether the final project requirements are to deliver register level C or assembler. If all programmers had to ''ask the internet'' they'd all be pretty worthless.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.