STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash Loader Demonstrator Code

Posted on December 02, 2014 at 14:39Hi,Does anyone know if ST have any resources that show how the flash loader works? I'm using ST's SPWF01S wifi module as a slave to an ST32F415 and I want to flash the wifi module(which is made up of an ST process...

RTC December read problem

Posted on December 03, 2014 at 19:49Hi.I have my RTC lib, which is working just fine except one thing.When december arrived, my RTC date register reads 0 as date except 12.I have read with RTC_GetDate(RTC_Format_BIN,..) and Month is set to 0.Why is ...

tm3341 by Associate II
  • 1239 Views
  • 3 replies
  • 0 kudos

Encoder Interface and Default_handler

Posted on November 29, 2012 at 13:48I'm trying  to read the tow signals from the encoder quadrature . I work with COIDE of coocox. but I don't know how i should write in the Default_handler (IRQ_TIM3). I want read the both edges of the encoder signa...

ahmed2399 by Associate II
  • 5911 Views
  • 16 replies
  • 0 kudos

STM32 Remap function issue

Posted on December 03, 2014 at 14:23Hi all, I'm working with stm32f103zhc6 mcu and the issue is that I cant write AFIO_MAPR2 register. Is the issue because the register exists in XL-density devices only or some special action should be applied to g...

Timer triggered DMA SPI stream

Posted on July 20, 2014 at 22:55 Hi guys! Is there anyone that has some experience in setting up this kind of DMA streaming? I would like to stream 16-bit data to an external DAC, with no sweat for the processor. I've read that tim...

How to send several frames through CAN

Posted on December 02, 2014 at 22:47I tried to send several frames through CAN of STM32F103R4 but i could only send one frame. Somebody know How to sende several frames? #can #stm32f103r4 #can

STM32F072x usart rx interrupt receive what I send to printf

Posted on December 03, 2014 at 05:10Hi ST,I connect my module usart tx/rx with STM32F072x PA10/PA9, and initial PA10&PA9 as usart1 to communicate with my module.Besides, I use printf to IAR Terminal IO window to debug, not redirect printf to usart1 ...

dqdqdq31 by Associate II
  • 1613 Views
  • 4 replies
  • 0 kudos

How to properly unlock a STM32F4xx device...

Posted on December 02, 2014 at 19:30Hello ST gurus! May I inquire on the right sequence of steps to unlock a device (level 1 lock) to unlocked (level 0)? The STM library reveals the following sequence is required to lock: FLASH_OB_Unlock();         ...

STM32F429 MDIO

Posted on December 03, 2014 at 09:47Hi,we have to manage a CFP Module via MDIO with STM32F429. Unfortunately the module requires MDIO according to 802.3 clause 45. I am right that the 429er supports only the older version (clause 22)?Is there anothe...

volker by Associate
  • 1056 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.