2014-12-03 12:47 AM
Hi,
we have to manage a CFP Module via MDIO with STM32F429. Unfortunately the module requires MDIO according to 802.3 clause 45. I am right that the 429er supports only the older version (clause 22)?Is there another possibility to avoid writing a bit banging driver?Did a controller of family STM32F4 supports MDIO clause 45?Thanks for help!Volker2014-12-03 1:24 AM
> I am right that the 429er supports only the older version (clause 22)?
Yes, the start and opcode bits appear to be ''hardwired'' to the cl.22 style.> Is there another possibility to avoid writing a bit banging driver?
Maybe SPI could be abused in some inventive way, but that may turn out to be close to pure bit-banging. > Did a controller of family STM32F4 supports MDIO clause 45? AFAIK, no. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.