2014-12-19 7:30 AM
Hello,
With the STM32F303RC, I use ADC12 in interleave mode with 2 DMA to reach a 10.2 Ms sampling rate.The ADC acquisition is trigged internally by TIM2 every 1ms, I read 1500 samples during ~100µs .That's was working fine until my code source size reaches a certain level.Now according the code size, I have often some ADC overrun.The issue is disapparing when either the code increase a bit or decrease a bit.When i used the ''not'' working binary with a STM32F303RE(512Kb flash, 80k RAM+CCRAM), I have never the overrunsThe current bin size is 233Kbytes, the RAM+CCRAM used is 30.3Kbytes, so that's below the limit ressource of the F303RC (256K flasn, 40k RAM+CCRAM).I already compared the (ADC12, DMA12, TIM2, NVIC) register settings before and after the issue but I found nothing bad.The current design requires a F303RC so I have to fix the issue.Any idea or suggestions are welcome to help me for this task.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.