8-bit data bus setting
Posted on January 21, 2015 at 21:34 hi all Where is my error check this code? How do I make an 8-bit data bus? thanks #include < stm32f10x.h > #include < stm32f10x_conf.h > #include < stm32f10x_rcc.h > #include < stm32...
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on January 21, 2015 at 21:34 hi all Where is my error check this code? How do I make an 8-bit data bus? thanks #include < stm32f10x.h > #include < stm32f10x_conf.h > #include < stm32f10x_rcc.h > #include < stm32...
Posted on January 20, 2013 at 19:48 Dear all, is there anyone knows how to add an integer to RTC_TimeTypeDef structure? For example, I have an RTC_TimeTypeDef variable 'timestamp'. After using the timestamp, I want to increase it by 45 se...
Posted on January 21, 2015 at 19:27Hi, I am trying to put the MCU in stop mode. I'm using the MCU STM32F072VBT6. The STM32F0 user manual says that the MCU can go in stop mode by executing WFI or WFE instructions with the SLEEPDEEP bit set in the sy...
Posted on January 21, 2015 at 18:38HII have Open Cortex-M4 Kits Open407V-D. I try to do an application resembling as proposed in this link. At the first part the LCD work correctly. But in the second part I have a problem when I want calibrate the s...
Posted on January 20, 2015 at 17:00Haw to configure the internal VREF (1.2V) for DAC usage. Regards Didi
Posted on January 21, 2015 at 00:27 I read absolutely all the posts in this forum plus some other posts online and I can't still make this work with IAR and the Terminal I/O screen. I can however make it work using the ST-Link Utility and...
Posted on January 21, 2015 at 11:57Hi I want to implement delay function using timer , as this has to be used with RTOS interrupt method is preffered and the Delay can vary from 500Microsec to 5.6Millisec. And this will be called at many location in...
Posted on January 20, 2015 at 13:40 Using the STM32F207, I am trying to get the DMA2 Stream 4 interrupt to fire. Can someone take a look at the setup below, and tell me if I have a problem with the setup? (I'm sure Clive will only have to take a...
Posted on January 19, 2015 at 20:18Dear All,I am working on a project where I want to control a couple of motors via CAN (CANopen).The STM32F407 is connected via an USB-Serial converter (FT232RL, FTDI) to a PC.(USART1 with USART_InitStructure.USART_...
Posted on January 10, 2015 at 00:05 Having trouble changing the STM32F4 clock (M4 clock) on the fly, dynamically. When I do, the target fails, sometimes not right away, but within a few dozen seconds. How do I know its failing? I have a task att...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.