font problem
Posted on January 20, 2015 at 15:41 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on January 20, 2015 at 15:41 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on January 16, 2015 at 17:13hello Every one I need 6 usart communications ; in stm32f407 we have only 4 usart and 2 uart Infact I still dont know the main diffirence between usart and uart ; so can I use uart as usart here ? Thank you in...
Posted on January 19, 2015 at 17:40The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on January 19, 2015 at 10:57Hi Guys,I previously had code working with Fatfs and I had LFN enabled but LFN_Unicode disabled. I now want to start using Unicode, but after enabling it in the ffconf.h file, my fat functions return FR_NOT_READY a...
Posted on January 12, 2015 at 10:52Hello, i'm using an STM32F407ZET6 with SPI1, SPI2, SP3 and SWD. SPI1 and SPI2 are always working fine. SPI3 works when the CPU is running without debugging. Whenever I set a breakpoint SPI3 Clock (PortB3) has stran...
Posted on January 16, 2015 at 22:06I can't seem to find the download software link for the CubeMX software? The link I have is here:http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?s_searchtype=partnumber This link only has do...
Posted on January 19, 2015 at 21:22The complete project is https://my.st.com//public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/49654/TIM8_OC.zip.I've made a simple test-program, which toggles some LEDs.I'd like PC6-PC9 to toggle automat...
Posted on January 19, 2015 at 21:19I've been reading through this (rather complex) datasheet for NOR flash.http://www.micron.com/~/media/documents/products/data-sheet/nor-flash/parallel/m29w/m29w128g.pdfIt's the same flash that the STM32F439xI EVAL ...
Posted on January 19, 2015 at 20:00Hello everybody! I've a very strange error. I've running application for stm32f407. I can download the code and it's working well. But when I want to debug with CoIDE the code stopped at 1FFF39c4 so in the system m...
Posted on January 01, 2014 at 14:22Hi all,I am a student who wishes to start off in ARM uCs with a small budget.I would like to know whether the STSW-MCU005 is supposed to be used with the AN2606 USART1 bootloader, so that i can use a USB-Serial dev...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.