2015-01-21 12:34 PM
#include <
stm32f10x.h > #include < stm32f10x_conf.h > #include < stm32f10x_rcc.h > #include < stm32f10x_gpio.h > #include ''fonts.h'' #include < stdio.h > #include < string.h > #define Set_CS GPIO_SetBits(GPIOC,GPIO_Pin_1); #define Clr_CS GPIO_ResetBits(GPIOC,GPIO_Pin_1); #define Set_RS GPIO_SetBits(GPIOB,GPIO_Pin_9); #define Clr_RS GPIO_ResetBits(GPIOB,GPIO_Pin_9); #define Set_WR GPIO_SetBits(GPIOB,GPIO_Pin_8); #define Clr_WR GPIO_ResetBits(GPIOB,GPIO_Pin_8); #define Set_RST GPIO_SetBits(GPIOC,GPIO_Pin_0); #define Clr_RST GPIO_ResetBits(GPIOC,GPIO_Pin_0); #define Set_LED GPIO_SetBits(GPIOB,GPIO_Pin_11); #define Clr_LED GPIO_ResetBits(GPIOB,GPIO_Pin_11); GPIO_InitTypeDef GPIO_InitStructure; //************************************************************************ void LCD_InitializePorts(void); void Write_Data(unsigned char data); void Delay(volatile uint32_t nCount); //************************************************************************* void Delay(volatile uint32_t nCount) { for (; nCount != 0; nCount--); } //************************************************************************* void Write_Data(unsigned char data) { Set_RS; Clr_CS; GPIOB->ODR = (GPIOB->ODR&0xff00)|(data&0x00ff); //PIN_0 1.2.3.4.5.6.7 Clr_WR; Set_WR; Set_CS; LCD_Delay(); } //************************************************************************* void LCD_InitializePorts(void) { GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); GPIO_StructInit(&GPIO_InitStructure); //PIN_0 1.2.3.4.5.6.7 LCD DATA PORT// //WR PIN 8 // RS PIN 9 // //LED PIN 11// GPIO_InitStructure.GPIO_Pin=GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7|GPIO_Pin_8|GPIO_Pin_9|GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); GPIO_StructInit(&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;//RST pin //CS pin GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); } //************************************************************************* int main(void) { Delay(0XF111F); LCD_InitializePorts(); while(1) { Set_LED ; Delay(0XF111F); Clr_LED ; Delay(0XF111F); } } //*************************************************************************2015-01-21 1:17 PM
Where is my error check this code?
How do I make an 8-bit data bus?
Lost something in the translation there.
The way you have the code set up the data bus is using PB0..PB7
Provide some context to your question, for example by diagramming how the LCD has been connected.
2015-01-21 2:58 PM
http://www.lovbuy.com/arduino2560-supporting-35-lcd-screenili-9327-p-7html?language=en
I first started The series stm32f I do not know how stm32f series data port. Is this code correct?GPIOB->ODR = (GPIOB->ODR&0xff00)|(data&0x00ff); //DATA BUSPORTB connected //PINS_0 1.2.3.4.5.6.7
thanks2015-01-21 3:11 PM
Yes, that would mask on the low order 8-bits to the Output Data Register (ODR)
The B Bank has 16 bits reflected on PB0 thru PB152015-01-21 4:16 PM
thanks
You're
my brother
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.