STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Setting the USART locks out the SWD function on STM32F030

Posted on January 22, 2015 at 17:32I am trying to set up a USART1 on a STM32F030C8 using PB6 and PB7. I can programme the part via the SWD, if it is blank or the USART have not been configured. As soon as I load code which configures the USART the p...

ihaslam by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos

STM32F4Discovery and USB VCP

Posted on January 17, 2015 at 07:18I'm trying to get the USB device virtual comport going.  I created a project with STM32Cube choosing Peripherals:USB_OTG_FS Device_OnlyMiddleWares:USB_DEVICE Communication Device Class (Virtual Port Com)Using Atoll...

AN3968 for STM32f4 discovery

Posted on January 22, 2015 at 08:05Hi All I am trying to update the firmware of my discovery board through Ethernet with the bb: DM-STF4BB. I have seen the http example of the AN3968, and that's what I want but the device libraries (stm324xg_eval.c)...

STM32F4 embedded bootloader problem

Posted on January 22, 2015 at 09:46 Can`t start the STM32F407VG chip in bootloader mode via USB. On the Discovery board all works fine if i set the boot0 and boot1 pins to boot from system memory. The device is enumerated in Windows as STM Devic...

vlpasha by Associate II
  • 13366 Views
  • 3 replies
  • 0 kudos

MIPI bridge chip for STM32

Posted on January 22, 2015 at 09:08I am looking for a bridge chip with which STM32 could allow us to communicate with external camera modules. However, after searching over Google, I found few products available. Since we actually need pretty high d...

chaoj by Associate
  • 968 Views
  • 1 replies
  • 0 kudos

STM32F407 Discovery w/ 3 Channel ADC and DMA

Posted on January 21, 2015 at 17:24 Looking through this forum I have seen the topic of ADCs and DMAs coming up a lot, and I apologize in advance for adding to it. but after reviewing most posts I still have not been able to implement ADC with t...

stm32f4 spi issue

Posted on January 21, 2015 at 22:37 I recently bought the STM32F429I-DISCO and less than one month down the line am beginning to get disappointed. I connected AT45DB041D to it via SPI5 and the last bit of almost every byte was misbehaving. Ei...

HAL and I2c problem

Posted on January 16, 2015 at 12:42I connect mpu6050 to i2c3 and make a project with stm32cube and enable i2c3. but cant detect sensor. for(i=0 ; i<255 ; i++)     {         test = HAL_I2C_IsDeviceReady(&hi2c3,i,10,100);         if(test == HAL_OK)   ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.