STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f3 Initialize DMA Transfer Complete flag ?

Posted on January 24, 2015 at 07:30 An odd question, maybe, but is it possible to initialize the DMAy_FLAG_TCx to true? I have a routine that teststhis flag and then sends data, and I would like it to fall through the first time. I'd rather not ...

STM32F107 SPI3 Remap

Posted on January 23, 2015 at 18:55Can some of the pins of a peripheral be remapped while others stay at their existing AF location?  I noticed in reference code on the STM32F107 that appears that some of the pins are remapped, but not all of them. ...

mvonahnen by Associate III
  • 753 Views
  • 1 replies
  • 0 kudos

Separate analog & digital supply MCU

Posted on January 23, 2015 at 10:051. I am using STM32 - 32 bit cortex M3, it has separate analog & digital supply pins.2. Datasheet says :VDDA and VSSA must be connected to VDD and VSS, respectively.3. Since I have 12 analog channels connected , so...

Wher is AN4514

Posted on November 06, 2014 at 11:03Hello, for the STM32F411, the new batch aquisition mode is announced. The datasheet tells that AN4514 should explain it, while the reference manual doesn't evne mention it. Any deeper information welcome! Thanks

STM32F207 SPI-Ethernet bridge maximum bit rate

Posted on January 23, 2015 at 15:43HiI'm using STM32F207.The task is to receive continuous stream of data on spi slave input at a speed of about 10-15 mbps. The data must be then buffered into the RAM and then transmitted as the packets over Etherne...

denisov by Associate
  • 669 Views
  • 0 replies
  • 0 kudos

Trouble reading STMPE1600_ID on STM324x9I-EVAL

Posted on January 14, 2015 at 23:20 I'm working with this board and the camera and a now modified derivative of the \STM32Cube_FW_F4_V1.3.0\Projects\STM324x9I_EVAL\Examples\DCMI\DCMI_CaptureMode project. When BSP_CAMERA_Init() callsBSP_IO_Init()...

hbarta2 by Associate III
  • 1844 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.