2015-01-27 8:53 PM
Hello,
I'm in the midst of project development using STM32F100RBx discovery kit (MB913C) and generating code by using STM32CubeMX and configure USART1 as asynchronous. I use Keil Arm-MDK and trying use ''HAL_UART_Transmit'' for transmitting 1Byte data but the result is wrong value. I had checked ''Target Configuration'' Tab using Xtal = 8MHz and HSE value like below : &sharpif !defined (HSE_VALUE) &sharpdefine HSE_VALUE ((uint32_t)8000000) /*!< Default value of the External oscillator in Hz. I need some advice if there are some wrong I do. Thank you Delau. #stm32We’re moving the ST Community to a new platform to give you a better and more reliable community experience.