STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Timer2 in Encoder Mode and CaptureCompare

Posted on February 02, 2015 at 10:21HiI use the Timer2 in Encoder Mode, works perfect. Now I need an Interrupt on a Compare Value if the Encoder rech this value, but the Timer should count normally. Eyample: Encoder Position = 1000 (Timer value) Enc...

dominik by Senior
  • 1054 Views
  • 2 replies
  • 0 kudos

SPI3 is not enabled ?!

Posted on February 02, 2015 at 14:15Hullo guys , I'm using STM32F429I , when i configure the SPI3 according this intialization RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2 , ENABLE); SPI_I2S_DeInit(SPI2);   SPI2_Struct.SPI_BaudRatePrescaler=Baud_Rate_...

STM32L0 compatible LCDs

Posted on February 02, 2015 at 09:39Hi, I'm searching for a LCD, witch is compatible with the STM32L0. I need to find a very cheap small Display. Of course I would prefer a character display. Is it possible to drive a character display without a con...

F334 HRTImer reset from TIM2

Posted on January 26, 2015 at 17:09 Hi, I need to generate a Signal with high resolution but with low frequency (sub 500ps resolution with frequency of 1kHz). My idea was to configure the HRTIMA in one shot mode (non retriggerable) and to...

PMW Timer Configuration Help Needed

Posted on January 31, 2015 at 16:24I am having trouble to get a couple of pins to toggle in PWM mode. It works, but there's a problem with the pin staying high. Here's what I am trying to do, it's quite simple, so I don't see why it is so much probl...

I2C communication: getting the wrong values!

Posted on January 31, 2015 at 22:43 Hei everybody, I am using a barometric sensor MS5611-BA03 for measuring the height. The sensor pressure values should be around 1000 mb, but instead of that I get -4895 mb. It's obvious, this can't be ...

esovo1 by Associate II
  • 1603 Views
  • 2 replies
  • 0 kudos

confusing about tpclk on page 662,RM0008 REV 15

Posted on January 31, 2015 at 13:44Hi,all.I am so confusing about the term tpclk on page 662,what does this PCLK mean exactly?pclk1 or just the word pclk?In my opinion,I guess the word tpclk represent 1/fpclk1,am I right? Thanks for hlep. #can #t...

346239463 by Associate II
  • 2379 Views
  • 4 replies
  • 0 kudos

STM32F103 Config & Read RTC

Posted on May 31, 2012 at 15:22 Hi, RTC works but i get only 1 second counter if i set RTC->PRLL = 0x32; below the init and get function. In most example i see 0x7FFF for PRLL. Why the counter counts slow.Any prescaler i missed? RCC...

Switching pin mode

Posted on January 31, 2015 at 19:13Hello, I have log. 1 on a pin and switch it off. After switching off I need immediately  measure voltage on this pin. How can I do this? One possibility is to configure pin to output, set log. 1, configure the same...

j3lda by Associate II
  • 1296 Views
  • 1 replies
  • 0 kudos

I2C problem, not getting the ACK bit

Posted on January 06, 2015 at 17:35 Hello, I am trying to communicate with the Barometric sensor MS5611, using the I2C protocol. My micro is STM32f3discovery. The address of the sensor is send, but not the command. The code is stucked in...

esovo1 by Associate II
  • 7442 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.