STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 Timer1 + DMA2 + SPI1

Posted on January 28, 2015 at 15:42Hello, is the following possible? Timer1 is in capture/compare mode. If an compare event is generated => start DMA2 DMA2 copy 2bytes in the data register of SPI1. SPI1 send the 2bytes I have try it, but I get no CL...

der-kyle by Associate II
  • 1481 Views
  • 2 replies
  • 0 kudos

STM32F407 FSMC To NOR Flash Issue

Posted on January 04, 2015 at 08:41The original post was too long to process during our migration. Please click on the attachment to read the original post.

shane by Associate II
  • 2952 Views
  • 5 replies
  • 0 kudos

Discovery boards and SPI/DMA example

Posted on January 28, 2015 at 23:47Hi folks,I'm working with two Discovery boards (STM32F4-DISCOVERY and STM324F429I-DISCO) I'm running the SPI DMA example (C:\STM32Cube_FW_F4_V1.3.0\Projects\STM32F4-Discovery\Examples\SPI\SPI_FullDuplex_ComDMA for ...

hbarta2 by Associate III
  • 967 Views
  • 1 replies
  • 0 kudos

STM32F427 data transfer in parallel from gpio using 8 ports

Posted on January 29, 2015 at 08:50HiI have some problems about transferring data.I want to send data in parallel from gpio 36MHz speed.I already set GPIO speed 100MHz.How do I set speed 36Mhz for transferring data in parallel?here is my codefor(i =...

dukesong by Associate II
  • 1655 Views
  • 3 replies
  • 0 kudos

STM32L053 Disco firmware image

Posted on January 29, 2015 at 19:39Hello, is there a imagefile  of the firmware on the L053 Disco available somewhere? I didn't find even after looking hard? Otherwise, can somebody send me that image? Thanks

Using the Timer BDTR Function

Posted on January 29, 2015 at 21:20Hello, Can someone please provide a brief explanation, and perhaps an example that demonstrates the BDTR in use? If it does what I am hoping: it may help to stop spurs being generated by the output pins when I swit...

Question about NRST pin on STM32F051

Posted on January 29, 2015 at 02:12We have a design were we are periodically going into stop mode, waking up on a RTC interrupt, running some code, then going back to stop mode.  Every time the processor wakes up, the NRST pin goes low for approxima...

mvonahnen by Associate III
  • 1322 Views
  • 3 replies
  • 0 kudos

Stm32F4 Lwip with enc28j60 ethernet module

Posted on January 29, 2015 at 18:51http://www.st.com/web/en/catalog/tools/PF257906I builded httpserver on this project then loaded to Stm32 but i couldnt take an ip adress from server. This project uses dp83848 module but i have the enc module. Is t...

Difference between ADC dual mode and 2 ADCs in independent mode

Posted on January 29, 2015 at 18:40Hello, I am using STM32F3 Discovery kitand I need to measure 2 signals at the same time. It seems to me that there are to possibilities: 1) use regular simultaneous dual mode, 2) use 2 ADC's, both in regular single...

j3lda by Associate II
  • 1467 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.