2015-02-02 5:15 AM
Hullo guys , I'm using STM32F429I , when i configure the SPI3 according this intialization
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2 , ENABLE); SPI_I2S_DeInit(SPI2); SPI2_Struct.SPI_BaudRatePrescaler=Baud_Rate_Prescaler; SPI2_Struct.SPI_CPHA=SPI_CPHA_1Edge ; SPI2_Struct.SPI_CPOL=SPI_CPOL_Low ; SPI2_Struct.SPI_CRCPolynomial=3; SPI2_Struct.SPI_Direction=SPI_Direction_2Lines_FullDuplex; SPI2_Struct.SPI_FirstBit=SPI_FirstBit_MSB ; SPI2_Struct.SPI_Mode=MASTER_SLAVE; SPI2_Struct.SPI_NSS=SPI_NSS_Soft; SPI2_Struct.SPI_DataSize=SPI_DataSize_8b; SPI_Init(SPI2,&SPI2_Struct);it is configured correctly , but when I enable the SPI by SPI_Cmd(SPI2,ENABLE);the SPE bit is not set and the MSTR bit is cleared (!!!!!!!!!!) When I call SPI_Cmd(SPI2,ENABLE); , before the initialization , the SPE bit is enabled Any help ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.