STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK_CLI Board Serial Number

Posted on March 17, 2015 at 18:40Hi, I have multiple STM32F4 discovery boards connected to the same pc. I use the ST-LINK_CLI utility to burn my user applications and reset them. Is there any way I can have access to the SN field that the ST-LINK_CL...

STM32L152 LCD driver

Posted on April 16, 2015 at 10:00Hello, I'm working on a custom board STM32l152 that include LCD (1/4 duty & 1/3 bias) I just want to enable all signal ( 64  =  16 * 4Com ) in order to check the screen. somehow only 1 (of 4) raw is working.   this i...

moran by Associate II
  • 1928 Views
  • 2 replies
  • 0 kudos

Availability STM32F411VxH

Posted on April 11, 2015 at 23:57Wiil ask my question here also because there's no reply form support to it: It's not clear to me if there will be an STM32F411VxH, that's the 100pin F411 in UFBGA100 package. Don't see it (anymore) on the product pa...

STM32CubeMX MDK-ARMV5 project generation problem

Posted on April 08, 2015 at 14:50Hi,I have a problem with MDK-ARMV5 project generation if the project is located on a network drive. Everything else is generated.If I have the project on a local disk everything works OK. I know that this is a simple...

blaz2 by Associate
  • 1781 Views
  • 3 replies
  • 0 kudos

Is my stm32f103 chip's execution speed too slow?

Posted on April 15, 2015 at 18:02Hi,    I have several time strict  TIMER ISR and I tested the execution time of one of them.The result is that 47 instructions(indluding 3 branch instructions) costs 3 us.My chip is stm32f103 and all code and data is...

360804365 by Associate II
  • 1936 Views
  • 5 replies
  • 0 kudos

ADC using DMA

Posted on April 10, 2015 at 12:25I'm using a stm32f429 running at 144MHz and I wanted to implement a periodic two-channel adc conversion. I need to make the conversions on a 1us period and I'm considering in using a dma adc conversion. I know how to...

damasosb by Associate II
  • 1821 Views
  • 3 replies
  • 0 kudos

needing low speed SPI communication

Posted on April 12, 2015 at 16:50Hello everyone! I am using STM32F103RET for my project. I need to communicate by SPI with a low speed digital device with the speed of at most 1KHz clock. At the same time, I need to have my own cpu clock as high as ...

abbas by Associate II
  • 1810 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.