2015-04-10 3:25 AM
I'm using a stm32f429 running at 144MHz and I wanted to implement a periodic two-channel adc conversion. I need to make the conversions on a 1us period and I'm considering in using a dma adc conversion.
I know how to make a continuous conversion using dma, but not a periodic one. If the conversion period was longer, I would use a timer interrupt to make a one-shot dma conversion, but been it a 1us period, I doubt the system can work at such speed. Can someone please give me some insight on the matter?2015-04-11 8:54 AM
A timer trigger to ADC1 which then also starts ADC2 in dual mode will probably solve the 1 us conversion requirement, and DMA can stuff the results in a RAM buffer. If this is continuous sampling, then your challenge is to process the results fast enough. If everything can be saved in a RAM buffer first, that is more do-able.
If this is a Disco board, use channels 5 and 13. Cheers, Hal2015-04-15 12:36 AM
I'm not sure if I understand what you are explaining to me. I should use a 1us timed interrupt that start an adc dual conversion using adc1 and adc2, is that it? I only plan to maintain this mode of operation during 15ms, so the results will be stored in a ram buffer and processed later, so that's why I'm planning to use the dma.
Could you please give me an example of configuration of the adcs and dma for this behaviour? I've never used the adc in dma dual mode, so I'm a bit lost here. Thanks in advance2015-04-15 7:08 AM
It looks do-able.
First refresh you memory with the F4xxx Reference Manual: Section 13.3 ADC Block Diagram identifies which timers have an ADC trigger Section 13.6 discusses external trigger Section 13.8.1 discusses using the DMA Section 13.9 discusses Multi-ADC mode Section 10.3.3 identifies DMA channel and stream selection Then the Standard Peripheral Library has an example of ADC Dual Mode Regular Simultaneous conversion. It may need some adapting for your application. The Hal library may also have something, but I am not familiar with that. Cheers, HalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.