STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 read analog signal

Posted on April 14, 2015 at 09:55HelloI have a nucleo STM32F103, I put a  external clock of 25MHz.How can i read a analog signal conected in PB8?Someone can help me??Best regards #analog-input #nucleo-f103rb

lemac by Associate III
  • 5004 Views
  • 7 replies
  • 1 kudos

SPI1 & SPI3 & JTAG

Posted on April 17, 2015 at 02:51Hello! I am fairly new to the specific Microcontrollers and of course to this forum, so first of all hello to everyone! Even though my question might be simple enough for most of you, I would like to express you my ...

pant by Associate II
  • 1568 Views
  • 3 replies
  • 0 kudos

STM32F072CBT6 Reset

Posted on April 17, 2015 at 10:48Hi thereI designed a print with a STM32F072CBT6 and connect with a Discovery Board.First I designed the software on the Discovery Board. After that, i want to test the connection to the CBT6. My Code works fine on th...

pfischer by Associate
  • 871 Views
  • 0 replies
  • 0 kudos

RM0090 published uart baud rates

Posted on April 14, 2015 at 06:06Hello, I have a stm32f429 discovery board. I am trying to confirm that I can achieve the max baud rates listed in the RM0090 document. I have tried using a pclk of 42 and 84 mhz, with oversampling of 8x and 16x. The ...

renasis by Associate II
  • 3164 Views
  • 8 replies
  • 0 kudos

My own BOOTLOADER with STM32F0

Posted on April 16, 2015 at 15:59Hi!  I'm  using MTF32F030R8 and I need to   develope  my own bootloader.  I use the first 8K of flash for bootloader (from 0x800000 to 0x8001FFF) and from 0x8002000 my SW  application. I'm not finding how to set the ...

lisa by Associate
  • 1492 Views
  • 4 replies
  • 0 kudos

PWM Input Capture via CH3 and CH4

Posted on April 16, 2015 at 14:12Hello I want to measure the duty cycle of an input frequency on the stm32f4. For that I need to use the TIM3 or TIM8 and there I have to use channel CH3 and CH4. But now I'm looking for TIM_PWMIConfig(...) and there ...

oli by Associate II
  • 3752 Views
  • 6 replies
  • 0 kudos

Boot1

Posted on April 13, 2015 at 16:50Where is the boot1 pin on STM32F3? More specifically STM32F334?

adaniel by Associate III
  • 1136 Views
  • 2 replies
  • 0 kudos

Power up STM32F407 Discovery using a 11.1V Battery

Posted on April 16, 2015 at 10:56Hello STM32-Community!I read in the document UM1472 that the 5V pin can be used as a input of an external power supply. I want to power up my board by using one battery (11.1V). I was thinking about a simple voltage ...

0690X00000605ZUQAY.png
yannick2 by Associate
  • 1256 Views
  • 1 replies
  • 0 kudos

STM32F4 8bit DMA to GPIO

Posted on April 16, 2015 at 17:05 Hello, I'm relatively new to the STM32F4 family but have worked with other microcontrollers in the the past. I'm trying to use DMA to send 8bits of data at a time from a memory array to a GPIO (GPIO_C) using ...

borisw37 by Associate
  • 1651 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.