STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power down reset feature to back up the external SRAM data

Posted on April 14, 2015 at 15:33Hi,I want to use external SRAM with the controller STM32F429. i want to make use of internal supervisor circuit, which is used to power the internal RTC and internal 4Kb SRAM, to backup the data in external SRAM. for...

vini by Associate II
  • 1515 Views
  • 2 replies
  • 0 kudos

Volatile uint8_t variable in interrupts

Posted on April 14, 2015 at 21:51 Hello, I have function fifo_read(RxFifo, &rx, 1) which reads byte from FIFO buffer. I want to use this function in two different interrupt handlers. I have declared rx variable as fo...

hospodar by Associate III
  • 2674 Views
  • 2 replies
  • 0 kudos

Debugger: Could not stop Cortex-M device

Posted on April 14, 2015 at 23:01I've made several custom STM32F4 boards.Never any problems, until now, when my JLINK detects my board ONLY, if I press reset button before I press detect device in Keil uVision.When I press download button I got erro...

tm3341 by Associate II
  • 1382 Views
  • 0 replies
  • 0 kudos

I Can´t disable RTC512Hz signal

Posted on April 14, 2015 at 17:03How can I disable RTC 512Hz signal and return PC13 as I/O ??I programed the PC13 as ''GPIO_AF_RTC_50Hz''  to calibrate the 512Hz signal of internal RTC, but now I cant disable it to use PC13 as I/O, The STM32F205 doe...

acer by Associate II
  • 1401 Views
  • 2 replies
  • 0 kudos

STM32L151 nRST pin... doesn't reset!

Posted on April 13, 2015 at 09:08We are experiencing a very annoying issue... we have a portable application, STM32L151, DVdd=3.0 regulated via an LDO, lithium battery. Randomly, the MCU freeze and the nRST does... nothing! We need a full power cycl...

eeprom emulation stm32

Posted on April 10, 2015 at 20:09  The original post was too long to process during our migration. Please click on the attachment to read the original post.

kemal by Associate II
  • 1637 Views
  • 4 replies
  • 0 kudos

USB DISCONNECT/CONNECT in STM32F107

Posted on April 14, 2015 at 04:51I am developing a HID USB with STM32F107, and iam currently using STM32_USB-FS-Device_Lib_V4.0.0. 1. My problem is that i dont understand clearly about USB_DISCONNECT feature in this MCU.2. I see in the library, ST d...

STM32F103VC UART5 problem

Posted on April 12, 2015 at 05:04Hi, I am trying to use UART5 on the STM32F103, 100 pin device. As per documents Tx and Rx pins are PC12 and PD2 respectively. I enabled clocks, initialized the port and when I try send a character (code below)      U...

nps by Associate II
  • 1617 Views
  • 4 replies
  • 0 kudos

STM32 LIN Documents Helping

Posted on March 24, 2015 at 02:34I am studying about LIN protocol and its implementation on STM32F107. Also I am new to this microcontroller, can anyone suggest me some materials about this microcontroller as well as the documents about LIN implemen...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.