STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDIO - 32F411 - Hw or Sw problem?

Posted on April 21, 2015 at 00:57Hi, I made a custom board to atach to a nucleo 411 board with a uSD shocket. I'm trying to get FatFs on it. I'v test almost every code on the web. I use System Workbench and Cube/stdperiph_lib. I would like a simple ...

STM32F3Discovery not connecting via USB

Posted on April 20, 2015 at 18:15Hi,today I tried to connect my stm32f3disco to my pc as usual, but for some reason it doesn't work. The COM led starts blinkin red and nothing happens. The message ''no st-link detected'' pops up either in keil or ST...

adriano by Associate II
  • 2057 Views
  • 4 replies
  • 0 kudos

Receiving CANbus data

Posted on April 22, 2015 at 01:27SO I am incredibly confused.  I have an application that uses CANbus.  I have the transmit running fine and I am to the point where I am receiving interrupts when I receive a message.  so I am confused by the lack of...

solsson by Associate
  • 693 Views
  • 0 replies
  • 0 kudos

Compensation for Flash Stalling on STM32F103

Posted on April 21, 2015 at 19:11Hello Guys, Working with multiple tasks in my project and one of the tasks measuring zero-crossings of power line mains with 5000 smaples/s and delivering detected zero-crossing to another task to be counted. I'have ...

STM32F429-Disco - TP - I2C

Posted on April 06, 2015 at 00:26Hello,I try to find some topick with same problem. But every topick is without the solution of problem.I have problem with I2C in 95% (yep, sometimes it works, after restart, it not work). I try to comunicate with ST...

feky2 by Associate
  • 1070 Views
  • 1 replies
  • 0 kudos

STM32F427 write to RTC Backup locations doesn't work

Posted on April 20, 2015 at 16:49I'm using the V1.4 version of the STMCube HAL driver to update the RTC backup registers. I can properly read and write to the Date & Time functions of the RTC.However, when writing to the RTC Backup registers, the da...

Trriger ADC injected

Posted on April 21, 2015 at 12:32 Hi, I would like to trigger ADC1 by TIM2 update. I checked and injected group workd fine by software triggering, i have checked in debug the sampled value. TIM2 cnt register also runs, so i p...

udibit by Associate II
  • 889 Views
  • 1 replies
  • 0 kudos

First step with Nucleo F091RC

Posted on April 21, 2015 at 10:35Hello everybody, I got a Nucleo F091RC and I'm starting programming but it is pretty complex. I use Coocox and GCC compiler. I try to understand how my board works with the HAL libraries. First I would like to cha...

raphael by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.