STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F427 FMC NBL0 NBL1

Posted on May 30, 2015 at 14:27Hi, I an laying down some decode logic for 2 x 16 bit SRAMs using Chip Select NE1, by bus configured for 32 bits 12 address lines. If I Write using address 0x60000000 the NBL0 and NBL1 signals are both low during the N...

Connecting COMP and DAC

Posted on June 01, 2015 at 22:00 Hello, I working with STM32F3, and my goal is to feed in an external voltage into COMP2 (non-inverting input) compared against another constant analog voltage (inverting input), in order to produce a calib...

theory by Associate
  • 786 Views
  • 0 replies
  • 0 kudos

Interrupt issue with timers and exti0

Posted on June 01, 2015 at 17:09Hi all, i'm new to cortex M4 STM32F4 processor and i have some problems with external interrupt handling and internal timer interrupt. Currently i'm trying this code on a DISCOVERY F4 board (with STM32F407) and i'm tr...

hexfet13 by Associate II
  • 1568 Views
  • 2 replies
  • 0 kudos

STM32L152-EVAL DFU example

Posted on May 06, 2015 at 13:10Hi All, I am attempting to update my STM32L152 board over USB using the DFU driver (STM32_USB-FS-Device_Lib_V4.0.0). I generated a .dfu file using ''DFU file Manager'' and the supplied binary_template project. I left a...

i2s full duplex DMA clarification

Posted on May 30, 2015 at 09:09hi everyone.for my application i need to use two microphones with PDM output (left and right).now i'm currently using one microphone, connected to a i2s in half duplex mode with DMA transfer (like the example inSTM32cu...

Timer 2 PWM and DMA not working

Posted on May 27, 2015 at 01:16  The original post was too long to process during our migration. Please click on the attachment to read the original post.

yoma1993 by Associate II
  • 4489 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.