STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuration timer interrupt 1ms

Posted on June 03, 2015 at 11:24hello,I use the stm32f103VD,Clock 48MHz from the 8MHz HSI.Can you help me and tell me if I configured the timer 3 correctly for counter each 1ms ?I am not sure it's correct because the iterruption comes each 0.000999 ...

SDRAM STM32F429 refresh problem

Posted on July 04, 2014 at 13:58The original post was too long to process during our migration. Please click on the attachment to read the original post.

m_ by Associate II
  • 4442 Views
  • 10 replies
  • 0 kudos

Avoid checking BOOT0, possible?

Posted on May 26, 2015 at 17:01I made a mistake of not putting BOOT0 pin connect to ground, which the STM32L051 MCU is not working at the moment.  Is it possible to rewrite the bootloader to I could avoid checking the BOOT0 pin for development purpo...

andy2 by Associate II
  • 1140 Views
  • 2 replies
  • 0 kudos

Trouble getting 800kHz from PWM timer and DMA

Posted on June 01, 2015 at 04:56 Hi guys, I've been trying to get this code working for the past week now and i'm out of ideas. I'm trying to control the ws2812 LEDs with PWM. These LEDs have tight timings and require a single 800kHz data...

yoma1993 by Associate II
  • 2886 Views
  • 4 replies
  • 0 kudos

STM32F use with serial ram, FMSC or DMA?

Posted on June 01, 2015 at 20:05I've got a 23LC1024 it's a serial ram with spi capabilities http://ww1.microchip.com/downloads/en/DeviceDoc/25142A.pdf I'd like to be able to use it as an extension of my addressable ram on the stm32fxxxx. I have two ...

sburr by Associate II
  • 2547 Views
  • 4 replies
  • 0 kudos

STM32F10B Eval Programming Issue

Posted on May 31, 2015 at 07:17Hi, I am using STM32f10B with STM32f103VGT6 on it. The problem is that the MCU is not working as per the program. It has a fixed GPIO high and they stay in the same state. I tried using coocox and IAR workbench. They ...

shauns87 by Associate II
  • 2502 Views
  • 5 replies
  • 0 kudos

stm32 UART-DMA one character transfer problem

Posted on June 01, 2015 at 14:21Hello! I'm using STM32F407 processor. When I'm trying to send 1 byte via USART-DMA (for example 0x72) I get two bytes ''72 72'' in terminal.If I send two or more bytes everything is okay. If I send something from term...

mdg82 by Associate
  • 1051 Views
  • 3 replies
  • 0 kudos

STM32F407 SPI-DMA Continuous Transmit and Receive.

Posted on May 27, 2015 at 12:11Hi, I am trying to configure the DMA based SPI communication for STM32F407. STM32F407 is the host controller(master), the slave is CC3100 WiFi module. I am implementing the DMA for SPI2. Following is my configuration c...

abhisheke by Associate II
  • 2734 Views
  • 6 replies
  • 0 kudos

STM32F4 FatFs f_open return FR_DISK_ERR

Posted on June 02, 2015 at 08:52 I'm using the FatFs library ver R0.10 to access the SD card. Here is my code: SystemInit(); USART_Configuration(); NVIC_Configuration(); /*-------------------------- SD Init ----------------------------- */ Sta...

Volatile variables causes issues with Coocox

Posted on March 21, 2014 at 10:34hello, I know that I should post this in Coocox forum, but I what to know if one of STM32 users faced this issue before: I have a strange issue with Coocox (COIDE V1.7.6), it may be a bug: - Optimization is set to -O...

moez by Associate II
  • 2889 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.