STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F10xxx TIMx PWM input mode

Posted on May 26, 2015 at 22:36HiI cannot find the STM32F10xxx firmware library as described here: http://read.pudn.com/downloads106/sourcecode/embed/437624/stm32/STM32F%20Documents/Application%20Note/STM32F10xxx%20TIM%20application%20examples.pdfI ...

STM32F103XX I2C Busy Flag after unsuccessful transfer

Posted on May 31, 2015 at 14:01Hi everyone. Did anybody deal with situation when I2C flag keeps being set after unsuccessful transfer (write). Lets imaging that your slave device is not connected right now or it fails to respond. First call to I2C->...

How to use STM32F4 to make floppy drive music

Posted on May 31, 2015 at 16:24Hello guys, I am new to this forum and I have a question for you experts. I would like to start this fun project where I would like to make ''floppy drive music'' Because the motor in the floppy drive moves it can prod...

theanswer by Associate II
  • 2832 Views
  • 6 replies
  • 0 kudos

lwip UDP disable CRC

Posted on May 31, 2015 at 01:33Hello!I am looking for an overhead free solution for UDP data streaming.Today I am able to stream UDP data from SPI->DMA->MEM->ETH, using pbuf by Ref:    TaskUdpStreamErr = netbuf_ref(buf, dataPointer, TASK_UDP_STREAM_...

ariel2 by Associate II
  • 1002 Views
  • 0 replies
  • 0 kudos

stm32f3 can't run 2 timer together??

Posted on May 26, 2015 at 05:58hello i have problem with my timer periph, i want to use 8 channel, so i use tim 3 and tim 4 together, but if i run the code together, it doesn't work, if i run just 1 timer(4 channel) its working correctly.. i have tr...

Interfacing Digital Temp. Sensor DS18B20 with STM32F051xx

Posted on May 30, 2015 at 07:48I tried to interface Digital Temperature Sensor DS18B20 with STM32F051xx but am getting struct in configuring the pin for the sensor. As in controller we doesn't have the dual mode so how we can configure single pin as...

sanchit by Associate
  • 1716 Views
  • 2 replies
  • 0 kudos

STM32F103, erase a function that define in spesial section

Posted on May 28, 2015 at 11:13hi in my software, define a section named ''My_SECTION'' and put just a function on it. in IAR .icf file define that section write in address 0x08050000. I used debugger, function is correctly wrote in 0x08050000 and h...

mn by Associate III
  • 1935 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.