2015-06-01 8:09 AM
Hi all, i'm new to cortex M4 STM32F4 processor and i have some problems with external interrupt handling and internal timer interrupt. Currently i'm trying this code on a DISCOVERY F4 board (with STM32F407) and i'm trying to use a delay function addociater to a button pressure (only to perform a anti-bounce function, without external capacitor connected ti user button) with this code:
void EXTI0_IRQHandler(){ NVIC_DisableIRQ(EXTI0_IRQn); EXTI_ClearITPendingBit(EXTI_Line0); btnPressed=1; delay_ms(100); NVIC_EnableIRQ(EXTI0_IRQn); } //interrupt every 1ms void TIM7_IRQHandler(){ TIM_ClearITPendingBit(TIM7, TIM_IT_Update); sysTimer++; if (!(sysTimer%100)) GPIO_ToggleBits(GPIO_LED,LD_GREEN);//alive led } Well, the code stops at ''delay_ms(100)'' function when i press the user button. This is bacause the sysTimer freeze it's content, because TIM7_IRQHandler isr is not server anymore. Inspecting the NVIC register i see the ISER0=10000040 before NVIC_DisableIRQ(EXTI0_IRQn) instruction and ISER0=10000000 . So timer2 and timer7 interrupts should works but this is not. Can anyone tell me why? where is the mistake?2015-06-01 8:23 AM
It's considered poor practice to use delays in interrupt code, especially ones dependent on other interrupts to function. Going to need to watch the pre-emption levels. Would recommend you read a free running hardware timer either a TIMx or DWT->CYCCNT and delta against the value in that instead of a variable.
Disabling this interrupt doesn't impact if others can fire, you have to return from this one.2015-06-01 10:15 AM
Thanks for your reply.
I was tring to disable the EXTI0 interrupt to prevent reentrancy to the same ISR caused by push button switch bounce; but the problem is that all other interrupt stops working: TIM7 does not increment sysTimer anymore and neither TIM2 works at all. I tried to modify the priority and sub priority af all interrupt sources without effect and then i tried to configure PriorityGroup adding this NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); before all definition of interrupts. And now, the program works as expected: i have the correct delay within EXTI0 interrupt. Thanks again!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.