STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 Usb Printer Device Class

Posted on June 03, 2015 at 21:02I'm developing a printer controller board (with STM32F070 mcu). Now I need to add  USB printer device. I'm using STM32CubeMX with STM32Cube_FW_F0_V1.2.0, but I don't found any examples about. Can anyone help me? Regar...

abci5961 by Associate
  • 1408 Views
  • 2 replies
  • 0 kudos

ADC conversion time STM32F303x

Posted on June 03, 2015 at 18:12What determines the conversion time of the onboard ADCs?I am having problems when I move from a MCU system clock frequency of 72MHz to 65.536MHz #adc #stm32f303

gbigden by Associate III
  • 1210 Views
  • 2 replies
  • 0 kudos

stm32f407 msc can not format

Posted on June 01, 2015 at 11:29 Hello!I am using stm32f407 flash to make a msc.It can be identified by my pc.But I can not format it.Can somebody help me?Thanks a lot!Here are my code on usbd_storage.c. /* Private typedef ---------------...

Can this be done with a STM32F103ZE

Posted on March 16, 2015 at 13:17Hello,I have no experience at all with micro controllers & only brief experience with wiring up electronics / & some low-level programming, so please accept my apologies up-front.I have a need to create a device that...

dubedat68 by Associate II
  • 6389 Views
  • 28 replies
  • 0 kudos

How to save time in production with STM32F429

Posted on May 25, 2015 at 14:22Hi,We are preparing production now. Because we use Unique ID to protect the products, each time we need to key the 96 digit Unique ID into the original file, then run the compile(rebuild), then flash into MCU. There is...

Linda by Associate II
  • 3002 Views
  • 15 replies
  • 0 kudos

STM32F469/F479

Posted on June 03, 2015 at 19:17Anybody noticed the http://www.st.com/web/en/press/en/p3678 of STM32F469/F479? They are F429/F439 on steroids: RAM increased from 256kB to 384kB, quad-SPI added, and - a specialty but maybe becomes ubiquitous soon - M...

Default frequency settings for STM32F4

Posted on June 03, 2015 at 17:43Hello!Until this time I did not called the so called Systeminit() function. Now I set up some frequencies for the clocks with the help of the clock_configuration xls. I would like to know what are the default settings...

janos by Associate
  • 1742 Views
  • 1 replies
  • 0 kudos

Generating trigg signals relative input capture

Posted on May 27, 2015 at 15:30Im trying to understand the input captre and output compare modes in the STM32 to fit my needs.This code is supposed be used in a shotdetector for droplets for our test equipmnet.Currently I'm using the STM32F3discover...

dangraf by Associate II
  • 3037 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.