STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Overclocking

Posted on June 04, 2015 at 09:39I'm using a stm32f303 which has a max clock speed of 72MHz. It would be very convenient for me to set it to 73.728MHz.  It works on my board, but what effect does a few percent overclocking have on the MCU? How is rel...

gbigden by Associate III
  • 4422 Views
  • 5 replies
  • 0 kudos

STM32F030 Internal Oscillator Accuracy

Posted on June 04, 2015 at 20:28I can't find the internal oscillator accuracy anywhere in the datasheet or the reference manual. If I have the sysclk set at 48MHz from the internal osc. what are the limits of what that sysclk may actually be? #da...

daniel2 by Associate II
  • 2389 Views
  • 5 replies
  • 0 kudos

Analog input pin for Discovery board

Posted on June 04, 2015 at 22:00I'm trying to get an ADC input to work on the Discovery STM32L053 board. The VREF calibration value is 0x68D, reading channel 17 shows 0x5E9, which by my calculations makes VDD 3.325 volts, which matches what I read o...

lee23 by Associate II
  • 1441 Views
  • 2 replies
  • 0 kudos

Flash Code Protection

Posted on May 29, 2015 at 02:55Hi,I am developing codes on STM32L0 microcontrollerI want to add flash read out protection function in the code.After I enable the PcROP(proprietary Code Read Out Protection), my codes do not work anymore. It does not ...

tianchen by Associate II
  • 3277 Views
  • 4 replies
  • 0 kudos

HAL Driver on STM32F051 and STM32L051 differences?

Posted on June 03, 2015 at 05:14 Must say the CubeMX generation tool is very good, and it really does make everything simpler. However, I run into a situation where I am using the STM32L051 and STM32F051 to test on a project connecting to the bl...

andy2 by Associate II
  • 1226 Views
  • 1 replies
  • 0 kudos

STM32F103 ADC internal band-gap (internal V-ref)

Posted on June 03, 2015 at 19:20Hi,For a project I need to use internal band gap (V-Ref). so i want to know how to: 1- turn-on internal band-gap voltage reference 2- select internal band-gap voltage as referencetanx all #adc #stm32f103 #v-ref

tux by Associate II
  • 1122 Views
  • 1 replies
  • 0 kudos

STM32f407 HardFault

Posted on June 04, 2015 at 00:35Can somebody explain me how to find cause of hardfault? I try to use solution from http://blog.frankvh.com/2011/12/07/cortex-m3-m4-hard-fault-handler/but buffer is empty.Here are core registers dump (from keil UI):SP ...

licencje1 by Associate II
  • 2181 Views
  • 3 replies
  • 0 kudos

error: No Cortex-m SW device found

Posted on May 14, 2014 at 15:07hi all, i was debugging happily my code on my new discovery F4 board when suddenly got this error please, could someone help me to fix this? may be that something burned inside my board? thank you so much Gio

0690X00000605YHQAY.png

STemwin GUI_Init Hard Fault

Posted on December 18, 2014 at 11:43Hullo guys , This is my first time to use STemwin GUI library , everything compiled fine , and the code is simple enough just to test it int main (){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE); GUI_Init();...

0690X00000602zKQAQ.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.