STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO port on fly selection mechanism in stm32f4xx

Posted on June 05, 2015 at 09:41HelloIf i want to connect output of an ADC(analog to digital converter) to two different ports, e.g. GPIOA and GPIOB, and to modify this selection by means of software code(no hardware modification needed), how is it ...

STM32F407 Discovery board to control bldc

Posted on June 05, 2015 at 18:28I am looking at implementing a 3 phase BLDC using hall sensor inputs and motor commutation on timers on the discovery 407 board. I have reference of http://www.mikrocontroller.net/articles/STM32_BLDC_Control_with_HAL...

gmali9 by Associate
  • 891 Views
  • 0 replies
  • 0 kudos

Problem with getting job

Posted on June 05, 2015 at 10:07Hello dear friends ! I working for freelance programmer microcontroller about 1 year . Today, I want to get formal employment in some companies . But employers are not interested in a freelance programmers , everyone ...

bomon85 by Associate
  • 1210 Views
  • 2 replies
  • 0 kudos

CCM and Structures

Posted on June 05, 2015 at 16:07 Hi everyone, I need to put the maximum of my data in the CCM. This is already done for simple types like this : uint32_t memory_dur_init __attribute__ ((section( ''.ccm'' ))); I'm scratching my h...

benoit2 by Associate II
  • 1055 Views
  • 1 replies
  • 0 kudos

STM32F205RCTb bootloader driver for Windows 7 64 bit PC

Posted on June 05, 2015 at 09:13HiOnce we jump to bootloader of STM32 controller for Firmware upgrade(DFU mode),the Windows7  64 bit OS  was not able to install driver automatically(However it worked in 32 bit OS). IS there any link or place where w...

stm32f4 USART2 problem

Posted on June 04, 2015 at 22:37 I am trying to use pb8 and pb9 with stm32f4 's usart 2 peripheral.I first used usart 2 with pb6 and pb7.It worked great but then i was obliged to change them. to pb8 and pb9. Here a quick look at my code. ...

d4ng3r09 by Associate II
  • 1293 Views
  • 2 replies
  • 0 kudos

USART1 - interrupt problem with STM32F051

Posted on June 04, 2015 at 17:01Dear community,I am trying to initialize the UART of the STM32F051 µC – however receiving of data does not work because the interrupt is not triggered. I recognized only the weak initialization of the UART1 interrupt ...

jogerh by Associate II
  • 1950 Views
  • 4 replies
  • 0 kudos

STM32F429 SPI Issue

Posted on June 04, 2015 at 06:39Just got a STM32F429 Discovery board and am seeing something weird when implementing an SPI driver in master mode. I'm writing the SPI driver code from scratch and am not using a peripheral library.The SPI peripheral ...

jerry2 by Senior
  • 1596 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.