STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Generate softaware interrupt..

Posted on June 08, 2015 at 10:48Hi, I want to generate a software interrupt,.. ie;when I execute one step it should go to ISR and do some activities.. My scenario.. I'm using RTOS for my application. I am reading data from a FIFO and storing it to a...

USB HID descriptor (problem with report id)

Posted on June 03, 2015 at 22:42 Hi, i'm trying to use USB device HID with a stm32F4 For this i modified the example give by st for HID standalone (not custom HID, didn't work for me !). If i use this descriptor i can send data to the pc : ...

idealsim by Associate II
  • 2005 Views
  • 1 replies
  • 0 kudos

GPIO (chip select) does not go high between SPI sends?

Posted on June 05, 2015 at 23:41I'm using SPI3 on an STM32F4, chip select toggled in software. I have a function that sets the chip select low, sends data and than pulls up chip select pin.Now I've noticed that when this send function is being calle...

input capture mode

Posted on June 05, 2015 at 11:29hej, i am getting a wrong values when i measuring the signal in input capture mode.can anyone help me what i am doing wrong and also i am new to this .i am using stm32f407vg the below oen is intialization. /new one  ...

arunl4g by Associate II
  • 2315 Views
  • 5 replies
  • 0 kudos

FM24C256 FRAM programming (STM32F0xx-DISCOVERY Board)

Posted on June 03, 2015 at 09:42 Hello dear members of forum, I would like to use a FM24C256 ram of RAMTRON ( http://www.kosmodrom.com.ua/data/memory/FM24C256ds_r3.1.pdf). I have tryed to write program for it but It do not work. When I...

STM32F407 SPI TXE flag Interrupt problem.

Posted on June 04, 2015 at 11:53Hi, I am using the STM32F407 SPI TXE and RXNE interrupts. The ISR checks if there is data to transmit or if any data is received. The data to be transmitted is filled outside the ISR and the TXE interrupt and CS is en...

abhisheke by Associate II
  • 2820 Views
  • 5 replies
  • 0 kudos

SPI_HandleTypeDef structure extern?

Posted on June 05, 2015 at 00:09I've used CubeMX to init SPI. There is a struct called hspi3 created by the init code which holds settings for SPI. I would like to use SPI library in a C file I've written (DAC driver) but I can't because HAL_SPI_Tra...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.